2015-06-05 9:28 AM
I am looking at implementing a 3 phase BLDC using hall sensor inputs and motor commutation on timers on the discovery 407 board.
I have reference of http://www.mikrocontroller.net/articles/STM32_BLDC_Control_with_HALL_Sensor In this the author suggests configuring the Timer1 as the commutation and Timer4 as the Hall sensor input. He also uses the Timer 4 channel 1 to capture time elapsed/speed in channel 1 and channel 2 to create dead time.... HOWEVER: When i try to configure the timers in STCube and once i configure the timer 3 (instead of 4 as it is taken by the discovery and makes no difference) to XOR ON combined channels, the channel 1,2 and 3 resources are taken away. Am I missing something? Are there any better non-confusing examples to implement BLDC with hall sensor inputs, It seems to me that this whole series is configured to enable these kind of controls, a good example will help a lot. Thanks in anticipationWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.