STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

confusing hardfault in STM32F407

Posted on June 14, 2015 at 16:59I get a hardfault in an STM32F407 I can't figure out. My speculation is that the processor tries to execute code beyond the flash end. The debug window says the following: Thread[1](Suspended: Signal 'SIGINT' received...

MB786.SchLib

Posted on June 16, 2015 at 12:23Hi everybody,I am working with STM3220G-EVAL board. Ihave downloaded the schematics of this board and I have modified them to adapt them to my project. The problem is that I can't find the library of the microprocesso...

i239955 by Associate
  • 1633 Views
  • 3 replies
  • 0 kudos

Timer speed/frequency STM32F411 - STM32F407

Posted on May 29, 2015 at 19:48In the datasheet of STM32F407 it is stated (Table 4, 2.2.21), the max speed for TIM1 is given with 168MHz, whereas TIM2-5 only run with max. 84MHz. This is quite clear, as TIM1 connects to APB2, running at max. 84MHz, ...

flyer31 by Senior
  • 10879 Views
  • 9 replies
  • 0 kudos

problem in running program with stm32f10rbt6

Posted on June 08, 2015 at 08:25hi every one i wrote a c project for a stm32f103ret6 in keil & download it with jlink v8 to mcu ,it work fine. but know i want to program same project to the stm32f103rbt6 but it dosent work correctly i download the p...

mhdizgah by Associate II
  • 3748 Views
  • 8 replies
  • 0 kudos

STM32 boot program

Posted on June 16, 2015 at 09:53Hi all, We had procured some sample STM32F105VCT6 ICs and were able to program the device through the serial port (USART1). Later we procured some from a local vendor. These are not getting programmed. On searching th...

nps by Associate II
  • 2057 Views
  • 7 replies
  • 0 kudos

Bug Report: CubeMX 4.8.0 with STM32F4 1.6.0 asserts from missing parameters in generated code + unused variable

Posted on May 30, 2015 at 00:30Here are a few parameters that are not filled in by the generated code that are then caught by the 1.6.0 library code:HAL_TIM_ConfigClockSource needs these values to be filled in with something:sClockSourceConfig.Clock...

Macro for accessing part of registers

Posted on June 16, 2015 at 12:35 This is not a question, just something I developed and I wanted to share with the community. I am fairly new to ARM and STM32 and perhaps there is some things I haven't come across yet. I realise that many...

angelos by Associate II
  • 1872 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.