2015-05-20 5:40 AM
i want to make two pulses tdelay1 and tdelay2 with different pulse width after rising edge of an external signal(let's name it sync pulse) also i want to calculate starting time of many signals
so i decide to use timers as a master and slave the best way that is in my mind is to use two timers(channel1 and channel2 in both timers because as i understand OPM is working in just channel 1&2 one as capture input and the other as pwm output) in one pulse mode to make those two signals and i also want to calculate starting time and pulse width of 6 signals based on Synced signals i also want to use just one interrupt in each cycle. and because of that i use a channel for rising edge and a channel for falling edge to calculate my desire. so i want to use those two timers as master to other timer(slave reset of the other) can OPM be Master? can Other OPM Channel Except 1 & 2 be used as input capture?2015-06-16 10:15 AM
Hello,
If you can refer to this two application notes available in ST website,you can found information about Timers interconnection.•http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00154959.pdf?s_searchtype=keyword•http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00156364.pdf?s_searchtype=keywordI hope that help,Syrine.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.