STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA FIFO Flush Issue

Posted on February 20, 2014 at 18:00I am using a STM32F4 as a SPI slave. The STM32F4 receives a packet of data over a USART line and must have the data immediately available for use in the SPI communication. I am using a DMA Tx memory to peripheral ...

szarovy by Associate
  • 2779 Views
  • 3 replies
  • 0 kudos

Programatically reading the state of a GPIO Output Pin.

Posted on June 16, 2015 at 10:45Hi,  I want to use the state of a GPIO Pin (It is driving a chip select on an SPI device) to determine that the SPI transfer has completed. I do know about the callback on the CMSIS code, but I'd prefer not to use tha...

Pevy.Andy by Associate III
  • 1806 Views
  • 1 replies
  • 0 kudos

Seperate file at flash memory

Posted on June 15, 2015 at 13:57hej i would like to keep some file in a seperate place at flash where linker dont use it when put the code in the flash.i am using COIDE., stm32f407 discovery board.Can anyone tell me how can i do that ?thank you.  

arunl4g by Associate II
  • 1783 Views
  • 9 replies
  • 0 kudos

STM32L053 Discovery Kit (UART between PC and Kit)

Posted on March 06, 2015 at 09:32Hi, i am very new to STM32, just installed the IAR environment. Appreciate if anyone could advise.Is there a UART example of String transfer using UART TX/RX of PA9 and PA10 in Polling mode  for STM32L053 Discovery K...

mark_ko by Associate II
  • 8699 Views
  • 29 replies
  • 0 kudos

Replacement for NVIC_SetVectorTable ?

Posted on June 16, 2015 at 01:35 In the latest HAL on the F1 (and F4) (http://www.st.com/st-web-ui/static/active/cn/resource/technical/document/user_manual/DM00154pdf ) Doesnt seem to contain NVIC_SetVectorTable(NVIC_VectTab_FLASH, USER_PROG_O...

STM32F405 Won't Oscillate ?!?

Posted on June 15, 2015 at 23:33Hello: This problem has me totally dumbfounded. Please see the attached image and screen shot of schematic. An absolutely simple circuit, yet it does not want to oscillate. This is the second board (different PCB, dif...

ADC Common Status Register

Posted on June 12, 2015 at 21:59The STM32F429 has three ADCs: ADC1, ADC2, and ADC3. They all have a status register, which has an EOC bit to indicate conversion complete.There's also a common status register (ADC_CSR) shared by all three ADCs that c...

jerry2 by Senior
  • 3078 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.