2015-06-14 7:59 AM
I get a hardfault in an STM32F407 I can't figure out.
My speculation is that the processor tries to execute code beyond the flash end. The debug window says the following: Thread[1](Suspended: Signal 'SIGINT' received. Description: Interrupt.) 5 irqGetStackFrame() irq.c:924 0x08028338 4 <signal handler called>() 0xfffffff9 3 <symbol is not available> 0x08563b54 2 movAvgFInit() util.c:346 0x08020e06 1 movAvgFInit() util.c:346 0x08020e06 The stack frame is: StackR3 0x10005cb4 StackR0 0x10005bcc StackR1 0x00000005 StackPC 0x08563b54 StackR12 0x00000000 StackR2 0x10005c0c StackLR 0x08020e07 StackPSR 0x21000200 stackframe 0x10006640 *stackframe 0x10005bcc The fault registers are: MMSR 00 BFSR 01 UFSR 0000 HFSR 40000000 DFSR 00000009 MMAR E000ED58 BFAR E000ED58 AFSR 00000000 In BFSR IBUSERR is set, as far as I can unerstand this probably flags the execution at 0x08563b54. In HFSR FORCED is set, looks like it's some problem with some exception handler. In DFSR HALTED and VCATCH are set, halt request in NVIC and vector catched event. The registers are: Core r0 0x10006640 r1 0x08563b54 r2 0x21000200 r3 0x10004788 r4 0x00000000 r5 0x00000000 r6 0x10005e2c r7 0x10005c0c r8 0x10005c64 r9 0x10005dec r10 0x10005bcc r11 0x10005dac r12 0x00000000 sp 0x10006640 lr 0xfffffff9 pc 0x08028338 xpsr 0x61000003 I have checked the interrupt vectors and they look ok.2015-06-14 8:31 AM
Problem with these things is that you need to dig interactively with the debugger/disassembler, and the stack content.
The LR of 0xFFFFFFF9 is a magic number controlling the IRQ/Fault returnThe PC is not good, and even, looks to have resulted from a BX R1You'd want to look at the code prior to 0x08020e07, ie movAvgFInit()Understand how it's loading the register, and if that's a result of a bad computation or a value held on the stack being corrupted.If there's stuff in the code you can sanity check, then do that, and add output to understand flow at/near the failure.2015-06-14 8:49 AM
Thank you for your advice. I will try to dig deeper...
2015-06-15 3:19 AM
Now I have digged into the problem and can draw a few conclusions, I think...
The problem is not related to movAvgFInit() util.c:346 0x08020e06, I have single stepped the assembly code and I'm almost certain it's OK. The problem occurs at other places as well. I added some code to toggle an I/O pin. The problem disappeared. I removed the code and expected the problem to return. It didn't. I think it could be some kind of weird timing problem causing an exception but can't prove/understand it and that makes me unhappy. Even more unhappy about the problem disappearing without explanation... I have read Joseph Yiu's book on the Cortex-M3 about exception handling but it hasn't helped so far. Any other recommendations?2015-06-15 3:30 AM
Using a GNU/GCC based tool chain?
Would double check the flash wait state and prefetch settings.You'd want to look at a disassembly of the code around the faulting location.2015-06-15 4:50 AM
Yes, I'm using GCC 4.8 2014q3.
I will check the flash settings. I have single stepped the assembled code at two of the locations where it failed. Thanks for helping!2015-06-15 5:18 AM
I have single stepped the assembled code at two of the locations where it failed.
Yes, but the debugger is going to distort the timing, and cache/prefetch behaviour. I'd do static analysis but have no visibility.2015-06-15 6:25 AM
My FLASH_ACR wasn't set up correctly. Or the debugger give me false information. I also found an error in RM0090, the location of the VOS bit.I will download new documentation and double check the settings.
What do you mean by ''I'd do static analysis but have no visibility''? I'm aware that you couldn't trust the debugger but I don't understand what you mean.2015-06-17 2:27 AM
Unfortunately I was completely wrong about the contents of FLASH_ACR, it was correct.
I looked at the wrong address, the RCC_CR. That explains the very strange value. The VOS error in RM0090 is not corrected in the latest revision, rev 9. Is there some place I can report it?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.