STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32H5 TIM Trigger GPDMA

You want to use TIM1 to trigger GPDMA to move the GPIOB->IDR data to a variable. The previous implementations were based on stm32L4, but I don't know how to implement gpdma. Attached L4 project.   *This post has been translated from Chinese to comply...

Resolved! about filter settings for receiving extended IDs.

HiI don't know how to configure the CAN filter bank registers to receive extended IDs in ID list mode.Naturally, I read the manual, but there was no explanation.Even if there was, it would probably be difficult to understand.  I found the following d...

c013.PNG
Ukazu by Associate III
  • 4046 Views
  • 5 replies
  • 3 kudos

Resolved! Unable to Debug, Break at address "0x80060c4"

Hey St Forum, Just getting a new project off the ground, and working with the STM32H7S7 Dev Kit. So far, I've been able to get some example code up loaded into CubeIDE, and upload to the board. However, when I try and debug, I get this error: Viewing...

halfordC_0-1721520992985.png halfordC_1-1721521055586.png
halfordC by Associate II
  • 2544 Views
  • 4 replies
  • 1 kudos

HardDefault when using DSP arm filter

Hi, I try to use arm_fir_f32 from CMSIS-DSP to bandpass my signal. But the program always run into the hard fault handler.I wonder if that could be i didn't correctly import the CMSIS-DSP library. I followed the instruction from https://community.st....

Jinchen by Associate II
  • 2367 Views
  • 4 replies
  • 1 kudos

USB OTG_HS_VBUS on STM32H series

Hi,I have a question about whether or not the USB VBUS connection needs to be made to the micro on the STM32H series micros (in particular the STM32H725) when operating the USB in device mode.We are using a USB-C type connection, so we have an indepe...

Resolved! stm32f4 interrupts and i2c

Hello;I'm writing a driver for a tlv493d magnetic encoder using CubeIDE. This encoder has a peculiarity where it pulls the SCL line of an i2c bus low when it has data ready to be read, at which point the MCU needs to initiate an i2c receive transacti...

sb_st by Senior II
  • 2928 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.