2024-12-10 10:09 AM
This code, partially generated by Copilot, does only print "="
At the same time, I do see that the device PB6(SCL) and PB7(SDA) recieves packets adressed to it, requestng data.
#include <Arduino.h>
#define I2C_ADDRESS 0x0B
volatile int x = 0;
volatile int y = 0;
volatile int add = 0;
void setup() {
Serial.begin(115200);
// Initialize LED pin
pinMode(PC13, OUTPUT);
// Enable clock for I2C1
RCC->APB1ENR |= RCC_APB1ENR_I2C1EN;
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN;
// Configure PB6 and PB7 as alternate function open-drain
GPIOB->CRL &= ~(GPIO_CRL_MODE6 | GPIO_CRL_CNF6 | GPIO_CRL_MODE7 | GPIO_CRL_CNF7);
GPIOB->CRL |= (GPIO_CRL_CNF6_1 | GPIO_CRL_CNF6_0 | GPIO_CRL_CNF7_1 | GPIO_CRL_CNF7_0);
// Reset I2C1
I2C1->CR1 = I2C_CR1_SWRST;
I2C1->CR1 = 0;
// Configure I2C1
I2C1->CR2 = 36; // APB1 clock frequency in MHz
I2C1->CCR = 180; // Standard mode, 100kHz
I2C1->TRISE = 37; // Maximum rise time
// Set I2C address
I2C1->OAR1 = (I2C_ADDRESS << 1) | I2C_OAR1_ADDMODE;
// Enable I2C1
I2C1->CR1 = I2C_CR1_PE;
// Enable ACK and POS
I2C1->CR1 |= I2C_CR1_ACK | I2C_CR1_POS;
// Enable I2C1 interrupts
I2C1->CR2 |= I2C_CR2_ITEVTEN | I2C_CR2_ITBUFEN | I2C_CR2_ITERREN;
// Enable I2C1 event interrupt in NVIC
NVIC_EnableIRQ(I2C1_EV_IRQn); // Enable I2C1 event interrupt address mached etc
NVIC_EnableIRQ(I2C1_ER_IRQn); // Enable I2C1 error interrupt.
}
void loop() {
static unsigned long lastPrint = 0;
if (millis() - lastPrint >= 1000) {
lastPrint = millis();
Serial.println("=");
}
if (add != 0) {
Serial.print("U:0x");
Serial.println(add, HEX);
add = 0;
digitalWrite(PC13, !digitalRead(PC13));
}
if (x != 0) {
Serial.print("U:0x");
Serial.println(x, HEX);
x = 0;
digitalWrite(PC13, !digitalRead(PC13));
}
if (y != 0) {
Serial.println("V");
y = 0;
}
}
extern "C" void I2C1_EV_IRQHandler(void) {
if (I2C1->SR1 & I2C_SR1_ADDR) {
// Address matched
(void)I2C1->SR1;
(void)I2C1->SR2;
add = 1;
} else if (I2C1->SR1 & I2C_SR1_RXNE) {
// Data received
x = I2C1->DR;
} else if (I2C1->SR1 & I2C_SR1_TXE) {
// Data requested
I2C1->DR = y;
//Serial.println(y); // Print the value of y
y = 1;
} else if (I2C1->SR1 & I2C_SR1_STOPF) {
// Stop condition detected
(void)I2C1->SR1;
I2C1->CR1 |= I2C_CR1_PE;
}
}
extern "C" void I2C1_ER_IRQHandler(void) {
// Handle I2C errors
if (I2C1->SR1 & I2C_SR1_BERR) {
I2C1->SR1 &= ~I2C_SR1_BERR;
}
if (I2C1->SR1 & I2C_SR1_ARLO) {
I2C1->SR1 &= ~I2C_SR1_ARLO;
}
if (I2C1->SR1 & I2C_SR1_AF) {
I2C1->SR1 &= ~I2C_SR1_AF;
}
if (I2C1->SR1 & I2C_SR1_OVR) {
I2C1->SR1 &= ~I2C_SR1_OVR;
}
if (I2C1->SR1 & I2C_SR1_PECERR) {
I2C1->SR1 &= ~I2C_SR1_PECERR;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.