STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RAMECC1 register reset value

Hi,MCU -stm32h743I have noticed that some RAMECC1 registers have a non-zero value on reset which is against the information given in the datasheet. For example, see the snapshot below:This is when the control is at the starting of main(). As per tabl...

Daan1_0-1732207430414.png
Daan1 by Associate II
  • 1271 Views
  • 1 replies
  • 1 kudos

Resolved! Undocumented behaviour STM32C011F4U6TR

Hi,We notice the startup time from power up can be affected by setting one GPIOB pin to input. The startup time here refers to the time from SystemInit() until main(). Basically it contains scatterload and __rt_entry to my understanding.Specifically,...

powerup_time_without_gpiob_input.png 2nd_iwdg_reset_without_gpio.png powerup_time_with_gpiob_input.png
ah2 by Associate III
  • 16966 Views
  • 30 replies
  • 2 kudos

Resolved! Does STM32H743 have integrated crystal load capacitors?

I notice that on the NUCLEO-H753ZI board schematic and BOM, the load capacitors are not populated for X2. My thought is that these caps must exist elsewhere, either built into the crystal, or integrated into the STM32H743.. But I do not see any menti...

BobaJFET_0-1733770911419.png
BobaJFET by Associate III
  • 1972 Views
  • 3 replies
  • 3 kudos

Resolved! Unable to modify RAM using ST-LINK_CLI.exe

I'm working with the STM32F407G-DISC1 development board. I would like to change the contents of RAM and hence I type ST-LINK_CLI.exe -w8 0x20000000 0xAB:ST-LINK_CLI.exe -w8 0x20000000 0xAB STM32 ST-LINK CLI v3.6.0.0 STM32 ST-LINK Command Line Interfa...

arnold_w by Senior II
  • 1229 Views
  • 1 replies
  • 0 kudos

stm32f465vit PA14 swclk pin always reset state.

Dear sir, madami use my new stm32f465vit with my custom Board swclk pin always reset state.PA14 swclk pin always reset state 0v, after i connect 10k resistor swclk and PA13 swdio pin to 3.3v. make it pullup also same PA14 is 0v (VCC)so, I can’t conne...

STM32H755 interrupt issue after secure boot (SBSFU)

I have a firmware running on an STM32H755. All working fine until I added a secure bootloader to the firmware and now the firmware crashes when initialising TIM3.My setup: STM32H755 on custom boardSBSFU (1_Image)Cubeprogrammer and CubeIDE.I've pinpoi...

tstokes by Associate III
  • 1228 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.