STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

quad_spi interface in F7 microcontrollers

Posted on August 20, 2015 at 09:14Hello. I'd like to know what microcontrollers has qspi interface? Whole STM32F7 series? The document DS10916 says that ''All STM32F75xx devices embed a Quad SPI memory interface, ...''(2.9.Chapter) but there is  no ...

Resetting a GPIO PIN INPUT

Posted on August 18, 2015 at 18:01Hello guys, I am using pin PC7 set has input on a http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1847/PF260320 and use IAR with . __HAL_RCC_GPIOC_CLK_ENABLE(); GPIO_InitStruct_C.Pin = GPIO_PIN_7; GPIO_In...

Protect my code STM32

Posted on August 19, 2015 at 15:16I am using STM32f407 and STM32f302 for a project and Finished, now I need to protect the code so no one can upload the hex from my controller ?? can anyone direct me where to look ? #read #flash #stm32f

kareemkna by Associate II
  • 2795 Views
  • 5 replies
  • 0 kudos

General question about Bootloaders and .hex/.bin files

Posted on August 19, 2015 at 14:01Greetings,I have a very general question regarding using an external uC, an EEPROM and an ethernet PHY IC to implement a reflash-through-ethernet capability on a custom board.My question is about the program data th...

bjerman by Associate II
  • 1191 Views
  • 2 replies
  • 0 kudos

void ADC_IRQHandler(void) Question

Posted on August 18, 2015 at 22:24 I think I know the answer but I just want to be sure. Is there any way to know from which ADC the handler is called? If I am using the 3 ADCs do I need to call the HAL_ADC_IRQHandler() for all like below? ...

keaven by Associate II
  • 1508 Views
  • 3 replies
  • 0 kudos

Virtual COM port driver windows10

Posted on August 18, 2015 at 13:28HelloI have a quastion about  Virtual COM port driver for windows 10.Windows detects port correctly but when I trying to use shows the message ''dangerously disconnected device''.The Microsoft suport told me thet is...

slawomir by Associate
  • 1032 Views
  • 2 replies
  • 0 kudos

UPS backup battery USB interface

Posted on August 19, 2015 at 11:49Hi all, did anybody connect UPS's usb interface into STM32F* USB host ? i'm having battery from APC and i have linux on machine that is having only serial interface, so i would like to use STM32F* to convert statu...

STM32F207 DMSBMR->SR always TRUE

Posted on August 18, 2015 at 13:41Hi all,I have a problem when I want to start-up my LAN board, the example program I used is STM32F2x7_ETH_LwIP_V1.0.2, after the program is running, the software reset polling flag ((ETH->DMABMR & ETH_DMABMR_SR) wil...

calvin by Associate III
  • 2557 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.