2015-08-18 4:41 AM
Hi all,
I have a problem when I want to start-up my LAN board, the example program I used is STM32F2x7_ETH_LwIP_V1.0.2, after the program is running, the software reset polling flag ((ETH->DMABMR & ETH_DMABMR_SR) will always TRUE.I browsed many similar post and inspected the clock source on the pins ETH_RXCLK,ETH_TXCLK and there are correctly sourced with 25MHz signal.
but the flag ETH_DMABMR_SR is still TRUE, are there any other ways I can debug my board?2015-08-18 5:00 AM
Have you enabled all 3 clocks in RCC?
RCC->AHB1ENR |= 0 | RCC_AHB1ENR_ETHMACEN | RCC_AHB1ENR_ETHMACTXEN | RCC_AHB1ENR_ETHMACRXEN ; JW2015-08-18 8:54 PM
Hi waclawek,
yes, as the original example code designed, the clocks RCC_ETH_MAC | RCC_ETH_TX | RCC_ETH_RX are enabled together. I describe my conditions more detail here, PHY mode is set as MII, I output a 25MHz clock from MAC to PHY_XI pin and observed the clock pins RX_CLK and TX_CLK both on PHY side and MAC side have 25MHz signal. As datasheet mentioned, RX_CLK and TX_CLK is generated by PHY, so I though PHY should be worked, the PHY I am using KSZ8721BTR.I don't know if there is another way I could debug my board, what else conditions toggle the DMABMR->SR flag?2015-08-18 10:47 PM
Besides setting all 3 clock enable bits in RCC, the only thing which comes into my mind is setting the two clock input pins to appropriate AF in GPIO_AFRL/AFRH and of course setting them to AF in GPIO_MODER.
JW2015-08-19 1:10 AM
Hi, I missed some AF configurations, now the SR can return to 0 and ETH_CONFIG is completed , thank you very much for the reminding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.