STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with UART2 output on new STM32nucleo board

Posted on March 14, 2014 at 04:56 I just got a STM32F103 nucleo board and am having issues getting UART2 enabled in my code to communicate with the PC through the ST-Link virtual port. UART2 is conncected to the ST-Link uart, which gets passed t...

toddberk by Associate II
  • 2596 Views
  • 3 replies
  • 0 kudos

Cube and #define USE_HAL_DRIVER...

Posted on August 20, 2015 at 09:16Hi,I'm using cube with HAL driver.. and need your help to understand the right way to include headers.I do not understand this example:I includes ''stm32f4xx_hal_adc.h'' ''stm32f4xx_hal_adc.h'' includes ''stm32f4xx_...

samuel23 by Associate III
  • 3684 Views
  • 4 replies
  • 0 kudos

Cube/MX frustration

Posted on August 05, 2015 at 23:18Hi STM32Cube/MX users,I've been using Stm32_StdPerihLib for years in dozens of successful projects. Now, after ST decided to replace SPL wir Cube I was ready to give it a try.My first impression was very positive - ...

osama2 by Associate II
  • 3344 Views
  • 7 replies
  • 1 kudos

Standarddeviation using DSPLib returns 0

Posted on August 19, 2015 at 15:02Hi,I have encountered the following problem on the STM32F4 using the CMSIS DSP Library V1.4.2:When calculating the standard deviation using arm_std_f32() of the following values </colgroup> 7111.15283 7111.3867...

USART DMA transmission

Posted on August 20, 2015 at 11:49Hello,i'm using the HAL library and CubeMx. The chip is a STM32F334C8.I want to send datas on USART1 with DMA control. The datas are well sent but when i go to the DMA complete transfer interrupt, i wait in the inte...

STM32F0 Nucleo(F070RB) board bootloader

Posted on August 19, 2015 at 13:09Hi, I am trying to connect to the bootloader on nucleo -F070Rb board. I tried the Flash loader Demonstrator, but I get ''No response from the target...''. I tried to send the start comman byte (0x7F) using realterm ...

seed by Associate III
  • 1911 Views
  • 4 replies
  • 0 kudos

Reconfiguring a Timer within its interrupt handler

Posted on August 18, 2015 at 20:59 On an STM32F4 Discovery (STM32F407) I'm trying to set up a timer and then reconfigure it within its own interrupt handler. The idea is that I should be able to repeatedly trigger tasks from the ISR in an...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.