2015-08-17 7:19 AM
Hi
Every time I rebuild my code using stm323cube my flash project settings change as default I always get this Programming algorithm STM32Fx4xx 2MB Flash 080000000H- 07FFFFFFFH but I need STM32Fx4xx 2MB Flash 080000000H- 081FFFFFFH As I am using a STM32F427ZITX processor so I have to added each time, Does anyone know how I change the defaults to stop this happening. I also need to reserve 0x81E0000 - 0X820000 as Non-volatile data store should I use the IROM2 area in the ''Target'' Tab or do I need to set it code some where, hopefully some one can point me in the right direction. Thanks John2015-08-17 8:57 AM
I think to goal of CubeMX is to generate a framework once, not over and over.
Changing the project meta-data is an aspect that has been poorly executed. Backing out settings you have changed even less well. If you're going to use CubeMX as an iterative tool, suggest you do that into a non-customized project and merge the output into your custom configured one.In things like Keil, I'd have to think you could just give the project file a different name, and then cube wouldn't over-right it, or place it in a directory that doesn't get erased/replaced.2015-08-19 2:48 AM
Hi owen.j,
1-080000000H- 081FFFFFFH does not correspond to 2MB 2-If you will use the IROM1 for data, you don't need to set IROM2 -Shahrzad-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.