STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f427 SAI Clock issues

Posted on October 30, 2015 at 14:55Hi I am struggling to get the External Audio Clock Input (PC9 12.288MHZ) to be output by the SAI Master clock pin PF7. I have used STM32Cube  to set it up and it all looks ok,  but I can not get any output on the S...

jowen by Associate II
  • 2085 Views
  • 3 replies
  • 0 kudos

STM32F7 EVAL to DISCOVERY project conversion?

Posted on August 11, 2015 at 17:48Hi, I'm trying to see some lwip examples on the STM32F7 Discovery. On that board, only one lwip application/example exists whereas for the EVAL board there are quite a few there covering many aspects of TCP/UDP/HTTP...

sv1eia by Associate II
  • 1516 Views
  • 3 replies
  • 0 kudos

STM32F7 DISCO - LCD_INT

Posted on October 11, 2015 at 14:47On the STM32F7-DISCO a signal from GPIO Port I13 LCD_INT connects to the 480 x 272 LCD.The STM32F745xx/STM32F746xx datasheet says that the AF14 mode of this pin is LCD_VSYNC. On the DISCO the LCD_VSYNC is on GPIO P...

STM32F469xx Data Sheet, Missing Data

Posted on November 01, 2015 at 17:20DocID028196 Oct 2015 Rev 2http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00219980.pdf Page 76, AF Table, Pin PG15, The FMC AF option is empty but should be FMC_NCAS

PWM Output on STM3210E-EVAL board

Posted on August 27, 2015 at 23:11 I'm trying to setup one of the LEDs on the STM3210E-EVAL board as a PWM output so that I can vary the brightness. I am targeting the red LED, which is on port F, pin 8. I have setup timer 13 which should be tie...

stm32f4 Help with CAN_ErrorCallback

Posted on October 10, 2015 at 20:29Hello.I have some problem and I can't do anything with it. So, I have CAN bus with two CAN. uP is stm32f407. When is normal work i send data by HAL_CAN_Transmit(&hcan2,5), and  HAL_CAN_Transmit(&hcan1,5). I receive...

[STM32F7 Discovery] - LTDC

Posted on October 30, 2015 at 20:28  The original post was too long to process during our migration. Please click on the attachment to read the original post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.