2015-07-26 2:01 PM
When code is regenerated from STM32cubeMX (4.8.0 & 4.9.0) for SW4STM32 toolchain, eclipse file link entries in .project become duplicated at the end of the file instead of replaced or updated. This does not yet cause a problem since eclipse appears to handle it by giving priority to the latter entries but if files have been removed in later configurations, the links in the project will still exists and be compiled. The workaround is to be sure to use version control, look at the changes to the link entries and manuallydelete the old file entries in the generated .project files to see what the differences are.
I have tried this on 2 different processors, the STM32F401RDTx and also with the default configuration for the STM32F429I-DISCO board.Reproduction:Start STM32CubeMX app (4.8.0 or 4.9.0)New ProjectChoose the STM32F429I-DISCOChoose project->Generate CodeProjectTab - project name is testProjectTab - ToolChain / IDE is SW4STM32Code Generator Tab - Select Copy all used libraries into project folderCode Generator Tab - Select Generate peripheral initialization as a pair of '.c/.h' files per IPCode Generator Tab - Select Keep user code when regeneratingCode Generator Tab - Select Delete previously generated files when not re-generatedChoose OK. Close STM32CubeMX. Observe and backup the file /test/test/SW4STM32/test Configuration/.projectOpen STM32CubeMX app.Open the test.ioc projectChoose project->generate code.Observe additions to .project file.Windows 7 x64. #stm32cubemx-eclipse-sw4stm322015-08-27 12:13 AM
Dear user,
This is a known issue that will be fixed in the release 4.10 coming out early september. Best regards2015-10-23 4:28 PM
It is still a problem.
I'm using STM32F7 discovery, CubeMX version 4.11
I went crazy after upgrade from STM32Cube_FW_F7_V1.1.0 to 1.2.0 it was adding another copy of every single file. I've solved generating the project from scratch and manually adding again my files.It worked for few times, now when regenerating it keeps adding 2 copies of stm32f7xx_hal_msp.c
It is a nice piece of software but the time you save in configuring the hardware you spend in making it work properly... Please fix it!!!2015-11-02 2:22 AM
Dear user,
The ioc attached is for F7 discovery and used with CubeMX 4. Can you please try it. We regenerated the code several times and did not witness any duplication. Thank you ________________ Attachments : TEST.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzFc&d=%2Fa%2F0X0000000bLr%2FTjgaWeiO28_XY5nhfSUje8NhighsW190ZhDABywB3Os&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.