2015-10-30 6:55 AM
Hi
I am struggling to get the External Audio Clock Input (PC9 12.288MHZ) to be output by the SAI Master clock pin PF7. I have used STM32Cube to set it up and it all looks ok, but I can not get any output on the SAI Master Clock even if i try and use the internal PLL clock. I am trying to communicate with a SSM2604 codec, I can see the clock is correct on the SAI_SCK_B (PF8) and I get a pulse on SA1_FS_B but SA1_MCLK is Dead I am using SAI_B in master mode with Master Clock Out. Any Help, examples etc would be gratefully received Thanks John #stm32-sai2015-10-30 7:14 AM
Hi John,
I'd highly recommend you to have a look to SAI_Audio example under STM32Cube F4 package: STM32Cube_FW_F4_V1.9.0\Projects\STM324x9I_EVAL\Examples\SAI\SAI_Audio, it can be very useful as starting example and it can be easily tailored to any other supported device and development board.-Syrine-2015-11-02 4:50 AM
Part of my problem is that the debug SAI section is missing for STM32F427ZIT chip I have reported this to ST and they are implementing a fix. So I rebuilt my code for the STM32F429ZIT so I could then play with the MCKDIV reg Currently it is set to 0 and the NODIV value is also 0 (the actual value of SAI_BCR1 is 0x001120C0) which should put the SAI_CK_B clock out on MCLK_B but it doesn't but when I change MCKDIV to a non zero value ie 1 I get a MCLK_B but divided by the MCKDIV so 6.144MHZ but I want 12.288MHZ any ideas?
2015-11-02 8:26 AM
Abit More info
Ok This is strange
if I use this code hsai_BlockB1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_96K; // SAI_AUDIO_FREQUENCY_MCKDIV; // then in debug manually set Mckdiv= 0x01 The MCLK Start working but if i set hsai_BlockB1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_MCKDIV; hsai_BlockB1.Init.Mckdiv= 1; then the MCLK does not start regardless of what I change in debug but if Initialize Block B1 with hsai_BlockB1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_96K; and then after HAL_SAI_Init(&hsai_BlockB1); set hsai_BlockB1.Instance->CR1=0x001120C1; MCLK works at half clock, I can not get it to run with Mckdiv set to zero But hsai->Init.AudioFrequency only appears to be used calculate MCKDIV but if it is not set to SAI_AUDIO_FREQUENCY_96K it does not work?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.