2015-08-11 8:48 AM
Hi,
I'm trying to see some lwip examples on the STM32F7 Discovery. On that board, only one lwip application/example exists whereas for the EVAL board there are quite a few there covering many aspects of TCP/UDP/HTTP/etc in Cube library. Is there a standard way to convert those EVAL application/examples to equivalents in Discovery board? Thanks for any replies. Christos2015-08-11 9:19 AM
The classic way would be to review the pin/hardware differences between the two, and adapt/port the initialization/configuration code accordingly.
It's not however unreasonable to expect ST to provide an equally rich set of examples for the DISCO board, as it's built as a full feature system, and the Ethernet functionality isn't achieved through some third-party board, or user modification.2015-08-11 9:42 AM
Hi Clive1
Thanks for taking the time to reply. I did give a try to the way you mentioned, yet it looks a bit difficult and time consuming since there are quite a few differences. In my attempt I got lost in the lwip required changes and I finally gave up. I do not know why ST ommited in CubeF7 library the lwip Disco examples as in Eval. Technology/Board-wise disco is absolutely capable of all of them without any addditional hw, strange! I'm interested only in lwip examples and the LCD for now. I know that the Disco has RMII so that should be one difference and the LCD I think is different, Disco's is 18bit Eval's 24bit. Anyway, if there is a simple point-by-point overview guide on how to do the conversion I could give it a go. Christos2015-11-02 7:08 AM
Did you have any look with this,
I'm looking for the sameBefore i give this idea up for dead and try a different platform ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.