2015-11-16 2:38 AM
Hello everybody,
I'm new on the forum and on ST microcontrollers.I'm trying to program the USART in assembly, but I have some issue to write on DR.What am I missing? Somebody can help me, please?********************************************* SECTION MYDATA:CONST DATATDR DCB ''HELLO WORLD!\r''; statup code....ldr r0, =0x40023800 ; RCC ldr r1, [r0, #0x10] ; RCC_AHB1RSTR bic r1, r1, #1 str r1, [r0, #0x10] ldr r1, [r0, #0x30] ; RCC_AHB1ENR orr r1, r1, #1 str r1, [r0, #0x30] ldr r1, [r0, #0x24] ; RCC_APB2RSTR bic r1, r1, #(1 << 4) str r1, [r0, #0x24] ldr r1, [r0, #0x44] ; RCC_APB2ENR orr r1, r1, #(1 << 4) str r1, [r0, #0x44] ldr r0, =0x40020000 ; Configurazione della GPIOA ldr r1, [r0] ; GPIOA_MODER bic r1, r1, #(15 << 2*9) ; Mask PA9/10 orr r1, r1, #(10 << 2*9) ; =AF mode str r1, [r0] ldr r1, [r0, #0x4] ; GPIOA_OTYPER bic r1, r1, #(3 << 9) ; Mask PA9/10, 0= push pull str r1, [r0, #0x4] ldr r1, [r0, #0x8] ; GPIOA_OSPEEDR bic r1, r1, #(15 << 2*9) ; Mask PA9/10 orr r1, r1, #(10 << 2*9) ; =fast speed str r1, [r0, #0x8] ldr r1, [r0, #0xC] ; GPIOA_PUPDR bic r1, r1, #(15 << 2*9) ; Mask PA9/10. =no pull ;orr r1, r1, #(5 << 2*9) ; =pull-up str r1, [r0, #0xC] ldr r1, [r0, #0x24] ; GPIOA_AFRH bic r1, r1, #(0xFF << 4*1) ; Mask PA9/10 orr r1, r1, #(0x77 << 4*1) ; =AF7, USART1 str r1, [r0, #0x24] ; Init_USART1 ; ; ldr r0, =0x40011000 ; USART1 ldr r1, =0xC00080 ; =reset value str r1, [r0] ; SR ldr r1, =0x683 ; =USARTDIV. per ottenere 9600bps a partire da HSI str r1, [r0, #0x8] ; BRR ldr r1, =0 ; =reset value str r1, [r0, #0x10] ; CR2. 1 stop bit ldr r1, =0x8 str r1, [r0, #0x14] ; CR3. =half-duplex selected ldr r1, =0 str r1, [r0, #0x18] ; GTPR. =reset value ldr r1, =0x2088 ; CR1. over=16, data bits=8, TE=1, TXEIE=1 str r1, [r0, #0xC] B main SECTION .text:CODE:NOROOT(2) THUMB main NOP LDR r2, =TDR ; carico in r2 l'indirizzo della base ; di memoria in cui è memorizzata la ; stringa ''HELLO WORLD!''polling ldr r1, [r0] ; USART1_SR ands r1, r1, #(1 << 7) ; se TXE=0 rimane nel polling beq polling ldrb r3, [r2], #1 ; carica il valore puntato da r2 e poi r2++ (byte) cmp r3, #'\r' beq main ; se sono uguali salta l'istruzione di memorizzare in USART1_DR ldr r4, [r0] strh r3, [r0, #0x4] ; scrive il dato da trasmettere nello USART1_DR B polling*********************************************ps: I'm modify the startup code given by STpps: I'm using IAR to write my program2015-11-16 6:01 AM
but I have some issue to write on DR
What does that actually mean? What issue? Your comments suggest you enable an interrupt, why would you do that, you have no handler, or NVIC configuration. The Nucleo's VCP port is USART2 PA2/PA32015-11-16 7:12 AM
My final goal is to use the USART to modify the duty cycle of a PWM waveform generated from a timer. In the final project I want to use the interrupts, so I leave the option for later on, but I know that option don't make any difference, because I need to configure the NVIC first.
Anyway my issue was in debugging mode, where I couldn't see the output on DR and the reset of TXE by hardware. After I wrote the post I decided to observe the output on PA9 with the oscilloscope and I was glad to see the USART working. I was stupid and a little bit lazy. Sorry!At the moment I'm trying to send data form PC and receive the same data from nucleosorry for my poor english2015-11-16 8:16 AM
Unhandled interrupts can result in the Cortex-Mx getting stuck trying to handle something that is never cleared, ie it never leaves interrupt state, and foreground code stops executing.
2015-11-16 8:18 AM
Peripheral register are not RAM, you often can't view the content written into logic structures that consume the data internally. In many cases the read and write view different registers.
2015-11-16 10:05 AM
Thanks Mr. Clive!
I appreciate your patience and kindness!I choose to leave TXEIE=1 to understand how interrupts works and seems if I don't configure the NVIC it doesn't matter if TXEIE=1 or =0next step. use interrupts to transmit/receive data from/to pc2015-11-18 1:27 AM
Hello everybody!
I wrote the code to send data from PC to nucleo and get back the same data from nucleo. I used as interrupt the RxNE flag.The code works ok and I would to ask you if I can improve my code to make it faster and more reliable.;***************************************************;;; Subroutines----------------------------------------------------------------- section get:CODE:NOROOT(2)get_char add r8, r8, #1 ldrb r3, [r0, #4] ; get char on r3 BX LR ; return from function call section put:CODE:NOROOT(2)put_char ldr r1, [r0] ; SR ands r1, r1, #(1 << 7) beq put_char ; polling on TXE add r9, r9, #1 strb r3, [r0, #4] ; transmit the data received on r3 BX LR;;; End Subroutines------------------------------------------------------------- SECTION .text:CODE:NOROOT(2) THUMB main NOP WFI ; MCU in sleep mode until RXNE=1 B main;;; Interrupts definition------------------------------------------------PUBLIC USART1_IRQ37 SECTION .text:CODE:REORDER:NOROOT(1)USART1_IRQ37 push {LR} BL get_char BL put_char pop {LR} BX LR;*****************************************regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.