2014-08-17 2:13 PM
I'm working on usb device project and I need after receiving a command from the host to return the device to predetermined state. To do this, all prepared OUT transfers must be canceled. I set endpoint disable bit(EPDIS) in the endpoint control register. USB core must generate endpoint disable interrupt, but this never happens. The interrupt is not masked. I checked with a debugger inside the interrupt service routine, that bit EPDIS remain set.
What I'm doing wrong? This is the code of endpoint disable function: void USB_OTG_DisableEP (USB_OTG_CORE_HANDLE *pdev , USB_OTG_EP *ep) { USB_OTG_DEPCTL_TypeDef depctl; __IO uint32_t *depctl_addr; /* Process for IN endpoint */ if (ep->is_in == 1) { depctl_addr = &(pdev->regs.INEP_REGS[ep->num]->DIEPCTL); depctl.d32 = USB_OTG_READ_REG32(depctl_addr); } else /* Process for OUT endpoint */ { depctl_addr = &(pdev->regs.OUTEP_REGS[ep->num]->DOEPCTL); depctl.d32 = USB_OTG_READ_REG32(depctl_addr); } if(depctl.b.epena) { depctl.b.epena = 0; depctl.b.epdis = 1; depctl.b.snak = 1; } USB_OTG_WRITE_REG32(depctl_addr, depctl.d32); }2015-11-18 9:02 AM
Hi,
i see the same issue on the ChibiOS OTGv1 driver. https://github.com/ChibiOS/ChibiOS/blob/master/os/hal/ports/STM32/LLD/OTGv1/usb_lld.c#L171 Also it seems that NuttX is working around this in their driver as well. Have you been able to solve this or find the reason for it? Thanks and cheers VincentWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.