STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two DMA captures For one timer

Posted on January 16, 2016 at 20:39I have a timer (Timer1) free running.I have assigned two input captures.when I run this code: HAL_TIM_IC_Start_DMA(&htim1,TIM_CHANNEL_1,&buffer1,20); HAL_TIM_IC_Start_DMA(&htim1,TIM_CHANNEL_2,&buffer2,20);only ''bu...

smhhadima by Associate II
  • 2914 Views
  • 6 replies
  • 0 kudos

HAL TIMER DMABurst Read

Posted on January 16, 2016 at 19:28does anyone have an example; how to use DMA burst with timer ''HAL_TIM_DMABurst_ReadStart''?*for any compiler*for any boardI just need to know how to use it #timer-dma-burst

smhhadima by Associate II
  • 1670 Views
  • 2 replies
  • 0 kudos

STMF030 ADC

Posted on January 18, 2016 at 16:42I am writing code for ADC in Assembly. Can anyone confirm or share an experience if there is a minimum latency or delay requirement after the ADC Cal routine is finished before ADEN bit can be set? I find I need a ...

STM32L053 HAL Multi Channel DMA ADC

Posted on January 18, 2016 at 19:07Hi,I'm having a problem getting the above to work with 2 channels using the cube generated code.I can get it to work on a single channel ADC, but not on multiple channels in scan mode.The HAL docs talk of ADC_Chann...

shorai by Associate III
  • 930 Views
  • 1 replies
  • 0 kudos

STM32F4-Discovery RTC only counting in debug

Posted on January 17, 2016 at 22:04 Hello. I am having a bit of a problem using the RTC in the STM32F4-DISCOVERY board. I am using the HAL libraries, and have configured the RTC using the LSI based on a number of examples I found online. Basical...

a60141 by Associate II
  • 2512 Views
  • 4 replies
  • 1 kudos

Precisely timed latching

Posted on January 17, 2016 at 09:21So I am running and STM32F0 at 48Mhz with TIM1 clocked to an external clock source running at 24.576MHz. On GPIO-A is connected a bus synced to the external 24.576Mhz clock. At occasional intervals I want to latch ...

luke2 by Associate II
  • 2398 Views
  • 6 replies
  • 0 kudos

DMA stm32f4 board problem

Posted on January 18, 2016 at 08:08Hi,I'm using the DMA to pass data from FLASH to RAM, on the stm32f4 board.transmission of 1500 Bytes.I've tried to send the data as byte,half_word,word,by casting and changing configurations (appears at the code), ...

haukeye by Associate II
  • 906 Views
  • 1 replies
  • 0 kudos

USART problem on STM32F415RG

Posted on January 15, 2016 at 16:04Hi, first to say that I'm beginner with STM32 programming, I study this uC entire month. I'm using board based on this http://www.mikroe.com/mini/stm32/ and I have limited (or no) support from manufacturer. I creat...

matke2002 by Associate II
  • 1755 Views
  • 4 replies
  • 0 kudos

more virtual com port questions

Posted on January 18, 2016 at 12:541. The current driver version is 1.4.0. But when I install this, and check the version in the device manager, it still shows as 1.3.1?2. Our system used to work on RS232, and was very robust. It is not as good on U...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.