2016-01-18 7:42 AM
I am writing code for ADC in Assembly. Can anyone confirm or share an experience if there is a minimum latency or delay requirement after the ADC Cal routine is finished before ADEN bit can be set? I find I need a minimum 125nS delay after cal routine before I can set ADEN bit to 1 and allow for ADRDY bit be set.
All provided examples are in C and each ADC configuration example program is executed with a function providing some amount of latency between called functions and a area ''For robust implementation, add here time-out management.'' I'm polling the ADCAL bit and finding I need 5 cycles (125nS) of delay before I can set the ADEN. If I do not insert this delay, program will loop and never receive an ADRDY. STR R0,[R1] ;MOVE ADC_CFGR2 DATA TO SELECT PCLK/4 ( SYS CLK = 40MHz/4 = ADC CLK = 10MHz) LDR R1,=0x40012408 ;MOVE ADC_CR ADDRESS TO R1 LDR R0,=2_10000000000000000000000000000000 ;ADCAL = 1 DATA STR R0,[R1] ;MOVE ADC_CR DATA TO SET ADCAL = 1 ADCE10 LDR R0,[R1] ;MOVE ADC_CR LOCATION DATA TO R0 LSRS R0,&sharp32 ;MOVE ADCAL BIT &sharp31 TO CARRY BCS ADCE10 ;WAIT UNTIL ADCAL = 0 TO CONTINUE DOWN LDR R2,=1 ;MINIMUM DELAY ROUTINE I ADDED BEFORE I SET ADEN CDLY SUBS R2,&sharp1 BNE CDLY LDR R0,=2_00000000000000000000000000000001 ;ADEN = 1 DATA STR R0,[R1] ;MOVE ADC_CR DATA TO SET ADEN = 1 LDR R1,=0x40012400 ;MOVE ADC_ISR ADDRESS TO R1 ADR0 LDR R0,[R1] ;MOVE ADC_ISR DATA TO R0 LSRS R0,&sharp1 ;MOVE ADRDY BIT TO CARRY BCC ADR0 ;WAIT UNTIL ADRDY = 1 TO CONTINUE DOWN, CODE WILL LOOP HERE WITHOUT ADDED CDLY #adc #assembly-instruction-set2016-01-18 10:57 AM
Well I think the Timeout is a different issue, and relates to escaping a loop.
You need to watch the fact that you're running the device at a fraction of the bus clock, and then pushing back-to-back transactions at that higher bus clock. There is no interlock here, so you need to give the slower device time to clock into its next internal state.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.