STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205 temperature sensor problems

Posted on June 24, 2011 at 15:06Hi everybody,I'm having some trouble with the STM32F205 temperature sensor. I'm using the algorithm from section 10.10 in the reference manual. {(V25 � VSENSE) / Avg_Slope} + 25I'm using the following algorithm to con...

tfk by Associate II
  • 7886 Views
  • 20 replies
  • 0 kudos

I2C Library

Posted on January 18, 2016 at 09:57Hi,I'm looking for a good I2C Hardware (no Software emulation) Library for STM32F3 device. I'm using the crossworks tasking library, so if there is anything which will bond with that, it would be great. I know ther...

manuel by Associate II
  • 946 Views
  • 0 replies
  • 0 kudos

STM32 Lifecycle.

Posted on January 16, 2016 at 23:51Hi, I'm new to the ST web site and I've been looking for information relating to the projected lifecycle of the STM32 cpu, predominately the medium density stm32f103 series. I want to know when its likely to be faz...

mbmail4 by Associate II
  • 3651 Views
  • 4 replies
  • 0 kudos

Win10 F4 USB CDC not data transfer

Posted on January 17, 2016 at 19:17Hello,I want to use USB to transfer data from temperature sensor. I have Win10. With CibeMX i create CDC device only program. I have installed ST Virtual Com Port Driver. When i run termital - it determine device C...

errors while using DSP lib

Posted on January 17, 2016 at 17:09 hi everyone I'm going to apply FFT on a signal captured by ADC but I've some errors I've tried to fix them but I couldn't can someone kindly help me with a solution. It is good to say that the errors are a...

ghfa0098 by Associate
  • 1367 Views
  • 1 replies
  • 0 kudos

flash memory endurance of STM32F030

Posted on January 17, 2016 at 03:08Hi~ I'm under review for EEPROM emulation on STM32F030. but, I found that flash memory endurance is min 1000 cycle(1K). Unfortunately, It is short to use in my project.Do you know why it is shorter than other STM3...

jaeshik by Associate
  • 1319 Views
  • 1 replies
  • 0 kudos

Input Capture module in pulse count example

Posted on January 16, 2016 at 07:49Hello all,In an external pulse count application, is it possible to capture Timer counts at fixed interval using input capture (IC) module while external input (TIM5_CH1) is driving timer time-base (through TI1F_ED...

rumlyen by Associate II
  • 2598 Views
  • 4 replies
  • 0 kudos

CubeMX and STM32L-Discovery

Posted on January 14, 2016 at 20:21Hi. I'am developer from Russia. And, i have a problem. I generate project in CubeMX with Virtual Com Port (USB 2.0) and upload it in my device (STM32L-Discovery board with STM32L152RBT6). When i connect USB cable (...

0690X00000602aoQAA.jpg 0690X00000602atQAA.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.