STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dual Interleaved ADC triggered by Timer with DMA

Posted on January 26, 2016 at 14:14Hi, I am using an stm32f4-discovery board and would like to acquire an reflected ultrasound signal with 4 MSPS. To generate the ultrasound signal two shifted pulse signals at 1 MHz are needed. The sampling frequenc...

0690X00000605KyQAI.png
smrtkai by Senior
  • 2044 Views
  • 4 replies
  • 0 kudos

Confusion between stm32l1xx_hal_usart.c and stm32l1xx_hal_uart.c

Posted on January 27, 2016 at 01:18Hi, can anyone clear up as to why, when I configure the USART2 interrupt  using the STM32CubeMX utility, the intialization code it generates calls functions in stm32l1xx_hal_uart.c instead of stm32l1xx_hal_usart.c?...

dean by Associate II
  • 2063 Views
  • 3 replies
  • 0 kudos

STM32L053R8 NUCLEO Bootloader firmware update issue

Posted on January 13, 2016 at 09:30Hi , I am encountering an issue with the firmware update using the bootloader. I updated my firmware using STMFlashloader Demo.exe. The new firmware is correct. My board is working. But when I use STMFlashLoader....

tingting by Associate II
  • 2931 Views
  • 7 replies
  • 0 kudos

F1/F2 Option Bytes

Posted on January 26, 2016 at 16:15I've recently changed from a F1 to a F2 uC in one of my projects. In the F1, there were two Bytes (Data0 and Data1) in the option byte register (FLASH_OBR) available for custom use (I used it to save a device addr...

FYI: STM32F4 discovery demo program

Posted on January 19, 2016 at 16:38I just got this board. When I tried the accelerometer part of the built in demo, nothing happened. The LEDS stayed blank. Otherwise the board started with all the 4 Leds blinking. As routine task I updated the ST-L...

LMI2 by Lead
  • 758 Views
  • 1 replies
  • 0 kudos

Bug Report: stm32f2xx_hal_wwdg.c

Posted on January 26, 2016 at 14:30Hello there, I was trying to activate WWDG using STM32CubeF2 v1.1.1 and got problems when trying to use HAL_WWDG_Start_IT. The handle was kept in lock state. Comparing with HAL_WWDG_Start I miss a call to __HAL_UNL...

PCC009V2 and EVAL6235N ?!

Posted on January 27, 2016 at 09:29Hi,We have purchased your Motor Evaluation Boards overDigikey.Products are PCC009V2 and EVAL6235N boards. A software CDnot included with packages. We cannot install USB drivers.Please contact us as soon as possible...

alpay by Associate
  • 832 Views
  • 1 replies
  • 0 kudos

stm32f429i-disc1 and breadboards?

Posted on January 15, 2016 at 22:27I thinking of ordering a stm32f429i-disc1 discovery kit and I was wondering how I can mount this on a breadboard as is has double rows of pin on both the left and right side?  The breadboards that I know of are mad...

bengt by Associate
  • 2726 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.