STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB transfer multiple of packet size

Posted on June 14, 2014 at 15:30I don't know whether this is related to the STM32CubeF4 package or the STM32F407 so I'll post here.I'm using the STM32F4 discovery board and the onboard USB FS port.I wrote a VCP interface that lets me send a buffer o...

shippo by Associate II
  • 9279 Views
  • 17 replies
  • 0 kudos

Upgrade from USB Host Library 2.0.0 to 2.1.0

Posted on June 24, 2014 at 18:02Hi guys,I recently upgraded my USB Host libary in one of my programs from version 2.0.0 to version 2.1.0 and it seems to have broken something. When I try to read a file from my USB Flash drive using FatFs, it crashes...

Why I can't use PA0 to get the function generator signal?

Posted on February 18, 2016 at 03:32I used a function generator send a signal to PA1, if PA1 get the high signal that let LED on. But my program can't work correctly. Always high or always low, depend on GPIO_Mode = IPU or IPD. Below are my program,...

SWD and JTAG

Posted on February 17, 2016 at 16:44I built my own board and I am trying to use the JTAG connections. It does not seem to work. It only uploads  a small percentage of time and even when it does, I am not to sure it is uploading correctly. I thought ...

achin by Associate II
  • 1847 Views
  • 5 replies
  • 0 kudos

JTAG without NJTRST

Posted on February 16, 2016 at 08:16Hello there, I have a general question regarding the NJTRST signal in a JTAG protocol. In STM32 datasheets, I read that JTAG can operate with only 4 pins, without NJTRST. I only assume it then uses regular #RESET ...

STM32F407VG with PS/2 Keyboard - project

Posted on February 17, 2016 at 11:48Hi, I'm second year student at UTP in Poland. I have to do project based on STM32F407VG. It's just simply communication with keyboard. But I have problem - power on my keyboard. I read that to power PS/2 I have t...

mich by Associate
  • 2046 Views
  • 3 replies
  • 0 kudos

STM32F405 I2S3 problem

Posted on February 17, 2016 at 17:58Hello,I'm having a problem after enabling I2S3 in master receive mode, for aquiring data from a mems mic.After calling HAL_I2S_Receive_DMA(), all other DMAs go to RESET state (all of them were READY).I tracked dow...

fb2 by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos

Measure 2 signals on TIM2 CC1, CC2

Posted on February 17, 2016 at 00:15Hi, On this link there's an example piece of code: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy.st.com%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcorte...

STM32F1 USART problem

Posted on February 17, 2016 at 18:38Hi, I am new to the STM32 family and I am stuck with a pretty basic problem. My board (STM32F105 CAN study board) came with a basic software in Flash, and I got the sources of that software which I am running from...

STM MCU with embedded 485

Posted on February 17, 2016 at 15:48Is there a STM MCU with RS-485 integrated on it ? It would be very usefull  given the fact that MCUs are industriall devices and one of the most used communication protocol in industry is RS-485.   

ionutF by Associate III
  • 1449 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.