2016-02-17 9:38 AM
Hi, I am new to the STM32 family and I am stuck with a pretty basic problem.
My board (STM32F105 CAN study board) came with a basic software in Flash, and I got the sources of that software which I am running from RAM. However, the USART2 does not behave the same from the source code in RAM. I.e., the code should output on USART2:++++++++++++++++++++++++ CAN Study Board++++++++++++++++++++++++But when I run the program 3 times in the following sequence:1. From Flash2. From RAM3. From Flash (again)the Putty output looks like this:++++++++++++++++++++++++ CAN Study Board++++++++++++++++++++++++▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒▒++++++++++++++++++++++++ CAN Study Board++++++++++++++++++++++++So the characters from the RAM implementation are corrupt. Any idea what the problem could be?2016-02-17 9:44 AM
Any idea what the problem could be?
Your RAM based code is built with the wrong HSE_VALUE defined?HSE_VALUE needs to match the speed of the crystal used in your design.2016-02-17 9:58 AM
YESSS!
Thanks for the extremely quick response, that was it!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.