STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 DISCOVERY KIT - USB JTAG Module Implementation

Posted on February 17, 2016 at 07:48Hello,We have an requirement for field program-ability using USB interface. Our SW development team already using ''STM32F4 DISCOVERY KIT'' for their development activities. Controller is STM32F407VGT6.The discove...

koyala by Associate
  • 1364 Views
  • 2 replies
  • 0 kudos

stuck on I2C_FLAG_BUSY

Posted on February 16, 2016 at 17:44Hello,I have try to send data from my stm to accelerator.The problem is when I check the flag before start to sending first command it stuck on busy.(I2C_GetFlagStatus) my pins are :D6, D7 (PINS that are free)What...

STM32F3 1.4.0 Firmware SPI Problem

Posted on February 14, 2016 at 19:11I am trying to use HAL_SPI_TransmitReceive() to read & write to a 25AA320A SPI EEPROM. The data was either read and/or written corrupted.  The data retrieved after a write was there, but the order was scrambled (n...

STM32 Nucleo Speed

Posted on February 17, 2016 at 07:46Hello and thanks alwaysI am currently using a STM32F091. In the specs I read that it is a Cortex M0 with 48MHz. My questions are:1) Can I be sure that it is running at that speed?  2) In general can the STM32 chip...

d_aliaga by Associate II
  • 795 Views
  • 1 replies
  • 0 kudos

STM32F0 EXTI Port unusable

Posted on February 17, 2016 at 12:50Hello,I noticed a problem with the STM32F030F4P6 Microcontroller.When I configure EXTI Line 0 and 1 with GPIOF =>PF0,PF1 are my EXTI for two Light Fork Barrier Modules.then all of the sudden my PB1 Pin can't be to...

Using math.h

Posted on February 16, 2016 at 15:49Hello every one I need to implement the code for STM32F, like the next lines: #include <stdlib.h> #include <math.h> ... int b; a= max(10, b) The compilation result is warning: implicit declaration of function 'ma...

tyr0 by Associate II
  • 4960 Views
  • 4 replies
  • 0 kudos

For ST: Reported HAL version versus Cube releases

Posted on February 12, 2016 at 02:21Hi,I noticed that the F4 release 1.11.0 code package uses a HAL Driver version number of V1.4.4. Is this intentional, and if so, is there a way to pull out the 1.11.0 number from some define?Andrei from The Great ...

STM32F1 ADC3 Issue

Posted on February 15, 2016 at 13:05 Hi, I am having problems Reading from ADC3. I have ADC1 and ADC3 set up on separate DMA channels. I have a separate task to fill a single array with both ADCs, however I can't get anything from ADC3, in fac...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.