STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error while erasing flash ROM

Posted on February 18, 2016 at 06:56I am using STM32F427IG microcontroller. The Flash Rom is connected to the FMC Controller.  I am getting error when I tried to erase a sector of flash memory. The error status flags- PGSERR, PGPERR was set. It work...

gigo by Associate
  • 1421 Views
  • 4 replies
  • 0 kudos

STM32F4 DSP IIR Filter

Posted on February 18, 2016 at 18:37Hello everyone, i try to make iir filter on STM32F4. Here how ive written it:float Sum,s1,s2, b0=3622,b1=7243,b2=3622,a1=822690,a2=-837162; int in0,in1,in2;in0 = ADC1->DR; // pass ADC -> circular buffer x1 Sum = 0...

F301 ADC injected conversion std peripheral lib commands

Posted on February 16, 2016 at 23:14I'd like get analog readings from pin PB0 triggered from timer 1 CC4, on my F301K6. I have configured the GPIO settings to set PB0 for analog input. There aren't any examples of injected conversion in the peripher...

avik by Associate II
  • 1899 Views
  • 3 replies
  • 0 kudos

BlueNRG DK 1.9.0 Projects not for Keil-ARM?

Posted on February 18, 2016 at 16:06Hi, I just downloaded the BlueNRG DK 1.9.0 to check the Nucleo Skin X-Nucleo-IDB05A1. Just to my surprise there all projects come only with IAR-EWARM Project files. Is this reality or STM really wants all Programm...

flyer31 by Senior
  • 918 Views
  • 1 replies
  • 0 kudos

HAL drivers SPI problem on STM32F4 Discovery

Posted on February 16, 2016 at 17:32 I have run into a problem when trying to setup a SPI com between the STM32F4 Discovery and a CR95HF RFID. The MISO data looks correct in the scope, however the software reads the bit 0 as 0 always, giving me ...

cesar by Associate
  • 1560 Views
  • 2 replies
  • 0 kudos

Using USB CDC as a passthrough to program another MCU

Posted on February 18, 2016 at 01:43I'm using an STM32F407 (#1) connected to PC via USB and another STM32F407 (#2) via UART3. I'm trying to program #2 via the bootloader using STMFlashLoader.exe by initializing #1 as a USB CDC device and passing thr...

jeffreyc by Associate
  • 1416 Views
  • 1 replies
  • 0 kudos

IAP: Boot Loader Write Protection

Posted on January 30, 2016 at 13:43Dear Forum Members, I am using STM32f103 custom board. I have divided my flash into 2 parts, one for custom bootloader and other for application(as explained in ST IAP example). Now I want to made boot loader secti...

Alternative Function

Posted on February 18, 2016 at 09:48Hi i wonder if it is possible to read the changes on the GPIO pin where the GPIO pin is configured as GPIO_Mode  = AF pin mode.  on f429?

arunl4g by Associate II
  • 850 Views
  • 1 replies
  • 0 kudos

STM32F4, HAL Lib, USART IRQ

Posted on February 10, 2016 at 09:40 Hi all, I'm working with STM32F4 mcu and keil uVision 5 IDE. I'm tryng to configure RS232 periph. but I have a problem. Transmission works fine but I'm not able to receive interrupt when something is recei...

tommaso by Associate II
  • 5022 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.