STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem reading SD card

Posted on March 11, 2016 at 20:08Hi to all, I have a big issue with SD cards. I initialize correctly my sd card, but when I try to read a block, I can read it only the first time. This is my routine: ===================== uint32_t MYSD::ReadSector(u...

STM32F4 synchronise timer + generate variable frequency

Posted on March 07, 2016 at 12:56Hi, I have a litte problem. I need to generate a variable frequency (not duty cycle) for a piezo buzzer. Unfortunately the PCB layout is givn as a H-bridge (see image). ''Piezo'' is connected to TIM4_CH1 and ''Piezo2...

0690X00000605b6QAA.png
kruszi by Associate II
  • 1250 Views
  • 2 replies
  • 0 kudos

F1 can hal_can_state always 0x22

Posted on March 11, 2016 at 21:36  The original post was too long to process during our migration. Please click on the attachment to read the original post.

bartocham by Associate II
  • 1482 Views
  • 2 replies
  • 0 kudos

Anomalous high ADC rate at stm32f103cb

Posted on March 11, 2016 at 21:02 Hello! I need an advice. My stm32f103cb chip has ADC with 0.39 us per point conversion rate on one channel. But datasheet says its max rate is 1 Msps (1us). I checked sampling rate with external oscillograph (1 ...

STM32F051C8 UART2 or 1 don't trigged

Posted on March 13, 2016 at 01:59 Hello i'm trying to configure an uart 1 or 2 interrupt in sw4STM32 and cube mx, but never responses the interrupt i can recive data from uart and send data in uart 1 and 2 in pooling mode mi code. Main ...

enagma by Associate
  • 592 Views
  • 0 replies
  • 0 kudos

send raw eth packets

Posted on March 12, 2016 at 07:47hi i am able to send/rec udp/tcp-ip packets on my stm32F4 via LWIP library and aid of cubeMX.i can see and track the transmitted packets from the STM32 board to pc (via wireshark) now i need to send some raw Ethernet...

STM32F1 SPI MOSI default pin level

Posted on December 15, 2015 at 01:42Hello, I want to use SPI to create a NRZ Style pattern. Everything is ok, except that I need MOSI to be low in between transmissions. Currently MOSI goes high after last byte shiftet out. I created a CubeMx projec...

taraben by Senior
  • 2577 Views
  • 3 replies
  • 0 kudos

STM32F4 SPI Busy Issue

Posted on March 11, 2016 at 17:20I'm using SPI in bidirectional 8 bit master mode to send 4 bytes to/from my control panel using HAL_SPI_TransmitReceive_IT(). When using SPI_BAUDRATEPRESCALER_256 it works fine, but smaller values cause the module to...

elmood by Associate III
  • 779 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.