STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f407 VG and VE variants

Posted on March 10, 2016 at 09:28Greetings,This will probably be an amateur question for most of you but I need to make sure.I have a project in which I use an stm32F407VGT6  mcu and I need to make another board.I don't have access to those mcus any...

azayetey by Associate II
  • 2197 Views
  • 1 replies
  • 0 kudos

I2C hangs after Pin reset.

Posted on March 14, 2016 at 16:47 Hi guys, I have maybe not a problem, but small issue with ST32F466RE nucleo board. I do some one way communication with a slave device (only writes). Everything works fine until pin reset. Power ...

pj by Associate II
  • 789 Views
  • 0 replies
  • 0 kudos

CS43L22 on STM32F4 disco-board

Posted on March 14, 2016 at 16:08Hi, It's about CS43L22 (Low Power, Stereo DAC w/Headphone & Speaker Amps) available on STM32F4 disco-board.So according to this schematic:

0690X00000605PzQAI.png

PWM output when CCR=0

Posted on March 14, 2016 at 16:07Hi. Ref. manual says that PWM output is '0' when CCR register is 0. I noticed a difference when I look output signal on a scope while CCR was set to 0. I have ARR set to 16383, timer frequency is 72 MHz. Thus, the pe...

matic by Associate III
  • 1170 Views
  • 0 replies
  • 0 kudos

using two probes

Posted on March 14, 2016 at 14:57Hello,I am working with ST-LINK/V2 and would like to use 2 probes simulteanously.The 2 probes are recognized with ST-LINK but I can't connect them simultaneously.I have tried to lauch 2 ST-LINk or to connect them wit...

LSE Intermittent

Posted on March 10, 2016 at 21:04Hello,I'm experiencing an issue with a STM32F101 using an 32.768kHz LSE.The LSE being used is the 7pf variant shown in the link below with 9pf caps as CL1 & CL2http://www.ecsxtal.com/store/pdf/ecx-71.pdfThe problem i...

patc by Associate II
  • 3151 Views
  • 7 replies
  • 0 kudos

output compare with 32 bit timer

Posted on March 14, 2016 at 11:19Hello there, I have a question regarding output compare mode with 32 bit timers in STM32F4 mcu. I have only one 32 bit timer that is free to use. I need to generate interrupts for 2 events. Those events should occur...

STM32F SPI DMA transfer, triggered by Timer

Posted on March 14, 2016 at 10:54Hi everyone, I have some cpu-load issue on my design, so I am trying to redesign an high frequency Rx spi transfer. (24bit) I would like to setup a timer that at a certain frequency triggers the Rx SPI transfer. Righ...

stm32f407 and 3g/gprs module ?

Posted on March 14, 2016 at 11:12Dear All,I am using an stm32F4discovery ( stm324f07vgt)  to capture images coming from a camera OV5642, i would like to send pictures ( 5MP) with 3G module, Could you please suggest me an exemple of module that suppo...

STM32F37x DMA SDADC + DAC same DMA Channel

Posted on March 11, 2016 at 17:03Dear Community, I am trying to use two peripherals (STM23F373) SDADC1 and DAC1_1 having the same DMA access channel: DMA2_Channel3 (STM32F37x reference page 164). Due to a synch problem I want to use the DMA in norma...

jogerh by Associate II
  • 1273 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.