STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading ADC after exactly 1.56 us

Posted on January 09, 2014 at 13:20The original post was too long to process during our migration. Please click on the attachment to read the original post.

sanjib by Associate III
  • 7738 Views
  • 21 replies
  • 0 kudos

stm32f100 pwm duty cycle

Posted on March 10, 2016 at 19:21I would like use the stm32f100 for buck loop control. In first, I reach to configure the timer and gpio to get a fixe PWM. But I don't know, for the moment, adjust or modify the duty cycle with a command. Before I u...

Troubles with priorities

Posted on March 09, 2016 at 17:25Hi there, can anyone help me with this??Im working with STM32f407.The programm consists in switch on/off lights and change its intensity using dimmer.A 50Hz wave is connected to a zero cross detector, and its output ...

miguel2 by Associate II
  • 2604 Views
  • 5 replies
  • 0 kudos

STM32L4 SPI DMA FIFO not writing into or corrupting memory

Posted on March 10, 2016 at 14:44Hi, I just wanted to connect a STM32 to a GPS using a SPI with DMA. Here is my setting : la : LOGICPORT LA1034 board : NUCLEO-L476RG mcu : STM32L476RGT6 gps : EVA-7M cube : 4.13.0 lib : HAL 1.3.0 clock : 80 MHz spi :...

Noyb by Associate II
  • 2193 Views
  • 6 replies
  • 0 kudos

stm32 discovery external supply problem

Posted on May 16, 2013 at 13:51I would like to program my stm32 discovery board via st-link, to do this i am trying to power my board externally by using 5V pin. However, when i powered the board, ld1 com turns red, but it blinks. In this case, the ...

asecen89 by Associate II
  • 4218 Views
  • 10 replies
  • 0 kudos

Why is PWM resolution twice shorter?

Posted on March 11, 2016 at 09:06 Hello there, I am trying to configure TIM1 and TIM8 for complementary PWM signals generation (in center aligned mode). It works, but for some reason my maxixmum PWM resolution is not 0xFFFF but 0x3FFF... I a...

Problem via SPI with STM32F103ZE and MCP4262 [Solved]

Posted on March 10, 2016 at 17:04I've the problem, my communication via SPI between STM32F103ZE and MCP4262 don't work.I try with PIC and the spi communication with MCP4262 works fine in mode 1,1.I try via SPI2 through GPIO pins from STM3210E-EVAL b...

vbruno1 by Associate III
  • 2678 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.