STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AHB transaction size

Posted on June 26, 2016 at 10:39i want to interface stm32f427 with 16 bit data bus external memories how can i change AHB transaction size to 16 bit ?

STM32F107 - mass storage device

Posted on June 17, 2016 at 11:06Hello,I am planning to build a device with a STM32F107, The user should be able connect to the system via both Ethernet and USB.When connected via ethernet, I should inform the IP address of STM32F107 to the user.For ...

rtursen by Associate II
  • 2763 Views
  • 8 replies
  • 0 kudos

STM32F437VIT6 = 168 MHz or 180 MHz ?

Posted on June 26, 2016 at 04:45We are looking at the STM32F437VIT6 and in the datasheet is saying the part has a max CPU frequency of 180MHz. I wanted to verify that the 180MHz was correct.When I checked the distributors online the part is listed a...

STM32F4 DISCOVERY Audio Playback

Posted on June 25, 2016 at 20:27Hello! Sorry if I repeat this topic. I have problem with BSP_AUDIO_OUT_Play() function from STM32Cube. Actually, i tried to run old example from StdPeripheralDriver-s package which plays sound from internal flash and ...

CAN bus on STM32F103

Posted on June 25, 2016 at 03:09Hi everybody, These days I'm starting a project based on STM32F103VET6 for which I have to use the CAN bus pheripheral to transmit and receive messages.  I'd like some support to start my work.- Can bus 29 bit identif...

doantt53 by Associate
  • 1804 Views
  • 3 replies
  • 0 kudos

STM32L0538-Disco Loses Programming

Posted on June 23, 2016 at 02:17When I connect my board to my computer via usb (cn2) I lose the programming. I lost the factory programming to start with. I downloaded the Keil uVision5 compiler and downloaded the blinky app to the discovery board. ...

About Alternate function AF14-STM32F4 Discovery

Posted on June 24, 2016 at 19:47Dear all,I am playing around with STM32F4 Discovery kit. In the manual RM0090, p. 270 mentions about the list of alternative fuctions.I have not found anything connect with AF14. Woud you please kindly help me to veri...

JTAG-DP in STM32F407: read+ APACC instruction returns zero

Posted on March 09, 2014 at 09:59Hello everyone, I use STM32F407 Discovery's JTAG-DP port controlled by basic TAP pins in my master thesis. I want to read access point's identification register (IDR) whose address is 0xFC. That's what I do, basing o...

natalia by Associate
  • 2083 Views
  • 3 replies
  • 0 kudos

STM32F769 Reference manual

Posted on May 02, 2016 at 08:50Hi, where can i find the reference manual of STM32F769? The STM32F7 page just contains the RM0385 which is applicable for STM32F75xxx and STM32F74xxx. Is this RM also applicable for the STM32F76xxx because it is not st...

sascha23 by Associate II
  • 2471 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.