STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C interrupt mode only works once?

Posted on June 21, 2016 at 14:53I follow the example of the I2C_TwoBoards_ComIT I have I2C host to send data to the STM32L4 board. The I2C slave has below logic HAL_I2C_Slave_Receive_IT(&I2cHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE); In the HAL_I2...

jiangpen by Associate II
  • 856 Views
  • 1 replies
  • 0 kudos

STM32 reading data from sensor through I2C

Posted on June 15, 2016 at 16:33Hello there! I have a running CPU and a sensor connected through I2C Interface. Everything is set in terms of hardware. Even the CubeMX configurations (startup codes) are implemented. However, I don't know how to gath...

[S] TIM2 - PWM Mode 1 - minimal duty cycle at 5kHz

Posted on June 23, 2016 at 10:55 Hi Guys, I am currently working on a PWM signal of f = 5kHz (T= 200us) with the 32-bit general purposte timer 2. While testing my implementation I am observing a strange behaviour. At the moment I am not sure i...

hof2 by Associate II
  • 3548 Views
  • 7 replies
  • 0 kudos

Problems using NVIC_SystemReset () and CAN bus

Posted on June 27, 2016 at 13:05Hi all,I'm developing an application with the stm32f103r8t6 where I've to reset the micro by CAN Bus and sometimes by pressing an external switch.To do that, I've written the following code:  RST_st = GPIO_ReadInputDa...

dsanchez by Associate
  • 813 Views
  • 0 replies
  • 0 kudos

UART only receive one data.

Posted on June 27, 2016 at 04:21Hello, I use STM32F303 Discovery board and try to test UART port.However, although I sent 5 sets of data, but the receiver port just only receive the first data. Does anyone know how to fix this issues?

yang2 by Associate III
  • 630 Views
  • 1 replies
  • 0 kudos

ADC with DMA triggered by software

Posted on June 22, 2016 at 15:32Hi,I would like to trigger the ADC conversion with DMA via a software command. I tried several configurations but I haven't succeed yet. The simplest thing would be to push a button and the ADC starts converting and a...

smrtkai by Senior
  • 3363 Views
  • 5 replies
  • 0 kudos

stm32f746-discovery

Posted on June 27, 2016 at 10:03Hello, I have a question about the demonstration code of stm32f746-discovery board. I can't see, in which file are defined the coordinates of touch buttons? #stm32f746-discovery

Suddenly - ST-Link Has Stopped Working !

Posted on June 26, 2016 at 17:50I have a problem here that doesn't make one shred of sense. I have boards (STm32F405VG) I programmed a couple months back that were fine. Meaning, I could connect to the board, and print the output statements from the...

EEPROM Emulation

Posted on June 26, 2016 at 11:59Can we interface external EEPROM with STM32f427 ? if yes can anyone please refer me some application note for STM32F427. I found AN3969 but it is for STM32f40x/stm32f41x and i need for STM32F427.

No ST-LINK detected

Posted on June 26, 2016 at 16:49Hello,I have a prototype board with:CP2102 USB - UART portSTM32F103RB(BOOT0 pin is configured highBOOT1 pin is configured low)Now I try to download some code to the board with Keil uVision.If I try to do it, the progr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.