2016-06-24 6:09 PM
Hi everybody,
These days I'm starting a project based on STM32F103VET6 for which I have to use the CAN bus pheripheral to transmit and receive messages. I'd like some support to start my work.- Can bus 29 bit identifier.- Are there any valid code example ready (Can bus 29 bit identifier) to download?-Could someone post me some configuration example?Thanks in advance! #can-bus2016-06-24 6:43 PM
Review available documentation and examples, including multiple examples on the forum, for filtering, etc. The CAN peripheral is very similar across many STM32 family members.
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\CAN\Networking2016-06-24 11:41 PM
I want to connect the CAN SAE J1939 network (29bit, 250KB / s). I want a sample CAN 29 bit. STM32F10x_StdPeriph_Examples\CAN\ Networking is 29bit?
Help me. Thanks2016-06-25 6:58 AM
The CAN peripheral can filter on the first 32-bits of the message, you will likely have to modify the examples to suit your specific needs. Start by understanding what you have, and then how you can get it to do what you need.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.