2016-06-21 5:53 AM
I follow the example of the I2C_TwoBoards_ComIT
I have I2C host to send data to the STM32L4 board. The I2C slave has below logic HAL_I2C_Slave_Receive_IT(&I2cHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE); In the HAL_I2C_SlaveRxCpltCallback, I set a flag to allow main loop to process the data. But it only works once, and the second time, it cannot receive data and cannot trigger the interrupt. May I know any other setting need to make I2C slave recieve multiple time? thanks #i2c-interrupts-stm322016-06-27 5:31 AM
Hi jiang.peng,
After receiving data the 1st time, are there any I2C flag errors set?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.