STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f4 timer output pin config

Posted on July 13, 2016 at 17:02HiI set timer 1 for output pwm on a pin.i need when timer is disable, pwm output will have ground level.when output pin is pull up and timer disable,output pin  have VDD LEVELwhen output pin is pull down  and timer di...

Keil with Cubemx

Posted on July 04, 2016 at 17:02I am trying to get the free Keil for stm32l0 tools to work with stmcubemx. In the 'Manage Run Time Environment ' dialog I expected to be able to select options for the stmcubemx framework API as described here :-http:...

Stm32User by Associate III
  • 1242 Views
  • 1 replies
  • 0 kudos

I have a problem with Option Byte

Posted on July 13, 2016 at 15:17 I can not handle the option byte as I would like. I use a STM32F103ZE, so with only one memory bank. I start from a state of write protection of all pages except the 60 and 61, then log FLASH_WRPR = ...

vbruno1 by Associate III
  • 1055 Views
  • 1 replies
  • 0 kudos

DAC waveform not displaying on oscilloscope.

Posted on July 12, 2016 at 04:56Hi ST community,     I'm doing a feedback of the adc output to the dac input to double check the incoming signal.    I seem to have a problem displaying the DAC(PA5) waveform on the oscilloscope, so my setup is : i co...

ADC Noise / Jitter Problem STM32F4

Posted on July 13, 2016 at 00:04I am using ADC's on the STM32F4 discovery board to read control values for my program from potentiometers and I am having problems where these inputs are very noisy, and cause my control values to modulate quite notic...

epalaima by Associate II
  • 1887 Views
  • 2 replies
  • 0 kudos

STM32F373CCT and CAN bus

Posted on July 07, 2016 at 19:24 Hello. I have CAN bus with three devices USB2CAN Adapter and two Controllers with STM32F373CCT. When only Adapter and one Controller is connected to CAN bus everything is correctly working. But if I have connect...

serg2 by Associate
  • 1173 Views
  • 1 replies
  • 0 kudos

Vrefint _Cal on stm32f103

Posted on July 12, 2016 at 11:42Hi I faced with a problem for read the Vrefint_Cal in stm32f103I dont find  Its address  in flash,I read  datasheet and also I searched in the internet but I cant find itcan you help me for sovling this problem???than...

STM32L152RE ADC

Posted on July 13, 2016 at 11:58I am using NUCLEO-STM32L152RE with 3 input channel of ADC and i used ADC in Interrupt mode with interrupt is generated after one channel conversion complete. And then in callback function of conversion complete i read...

djtilava by Associate II
  • 891 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.