STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN Driver bug (?!)

Posted on April 16, 2015 at 16:42I think i found an bug in the CAN driver. Explain me this:a) Receiving 1. In the example application HAL_CAN_Receive_IT is called from HAL_CAN_RxCpltCallback 2. Looking in the implementation of the driver we see that...

STM32L073 NAND flash wear leveling code

Posted on July 14, 2016 at 13:02Hi, I am working on STM32L073 board with a SPANSION NAND flash memory. I would like to implement a wear leveling system to it but seem like there is no example code inside the STM32CubeL0. Is there any wear leveling e...

waiyang93 by Associate II
  • 1599 Views
  • 1 replies
  • 0 kudos

STM32F746 FMC Issues

Posted on July 14, 2016 at 14:51I have a Spartan-6 FPGA connected to an STM32F746IG using the FMC. The FMC is configured for SRAM in region 1.1 (0x60000000). I have disabled caching of the FMC region in the MPU. I see FMC read & write cycles with th...

kurth by Associate
  • 797 Views
  • 0 replies
  • 0 kudos

response to ''HAL Code Quality''

Posted on July 14, 2016 at 14:16Hello Mayla,here are some examples:*  If there is a function that can not fail, please use void as return type:„HAL_StatusTypeDef HAL_DeInit(void)'' should be „void HAL_DeInit(void)“. If the software does not contain ...

torsten2 by Associate II
  • 770 Views
  • 0 replies
  • 0 kudos

STM32L0 complementary PWM

Posted on July 13, 2016 at 14:47Hi everybody, in the datasheet of the STM32L073VB, it says there is no advanced timer with complementary PWM output. Still we need two complementary outputs, very simple without delay function. Is it possible to use a...

USB MSC library - null pointers

Posted on July 11, 2016 at 08:28In the file ''usbh_msc.c'' generated by CubeMX there seem to be various instances of null pointer dereferencing. Many functions begin with this statement: MSC_HandleTypeDef *MSC_Handle =  (MSC_HandleTypeDef *) phost->...

STM32F4xx, CCMRAM startup init

Posted on July 09, 2016 at 22:17 Hello guys, Encountering the following problem: static __attribute__((__section__( ''.bss_CCMRAM'' ))) int data; ''data'' is put explicitly into CCMRAM (verified with debugger) bu...

sony_nix by Associate
  • 1397 Views
  • 2 replies
  • 0 kudos

STM32L073 store data after power off

Posted on July 12, 2016 at 11:19Hi,I am working with an external flash and I wanted to store the lastest memory address after the power cut off and fetch back the stored memory address when power on. So, how should I do it ?  Is it done by write int...

waiyang93 by Associate II
  • 12447 Views
  • 12 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.