STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC timer is unstable in simulation

Posted on July 08, 2016 at 13:13Hi Team,Use RTC as timer to restart STM32F030K6 from stop mode every 10mS, Set/Reset a dedicated I/O to show stop and running duration respectively in main loop like following procedure.  while(1){ if( RTC_Refresh_Tim...

jhl14 by Associate II
  • 2116 Views
  • 4 replies
  • 0 kudos

STM32L053 Discovery IAR Project

Posted on July 13, 2016 at 10:52Hi, I am new to STM32 microcontroller and I am after a bit of guidance with respect to starting projects in IAR using this microncontroller. I have a STM32L053 Discovery board and I have been working through the examp...

STM32L476 USB device does not work

Posted on July 07, 2016 at 17:08I've a big problem to make USB device working on STM32L476 device. I've tried my board, STM32L476 discovery and the results are the same, so I gues it must be firmware issue. I've used code generated from ST Cube and ...

krestan by Associate II
  • 2412 Views
  • 3 replies
  • 0 kudos

Custom USB storage based-on STM32F7.

Posted on July 08, 2016 at 06:31Hi all, I'm developing custom usb mass storage using stm32f746 + MT29F64G08CF MLC NAND. Can you show me low-level nand driver of Cube Firmware support for this NAND ? I can run usb mass storage using sdcard on stm32f7...

STM32 FMC Display

Posted on July 12, 2016 at 08:23Hi everyone, I have a display hooked up to an STM32F767 via the FMC and all is working properly.  When I try to use DMA2D the DMA2D will only transfer the first 64K of data.  There is no error generated, it appears to...

gvigelet by Associate II
  • 2080 Views
  • 3 replies
  • 0 kudos

STM32L1 HSE/PLL failure

Posted on July 11, 2016 at 13:56Hi,2 questions about HSE/PLL :1. Supposing the HSE/PLL is running fine, is it possible that it suddenly stops running without any reason ?2. If yes, what happens about the SYSCLK ? Does it switch to HSI ?Thank you for...

Kuikui by Associate III
  • 2386 Views
  • 4 replies
  • 0 kudos

Registers datasheet

Posted on July 12, 2016 at 17:42Hi, I am currently using the STM8L152C6 MCU but I can not find the datasheet about registers.I looked at all datasheets present on this http://www.st.com/content/st_com/en/products/evaluation-tools/product-evaluation-...

0690X00000605bGQAQ.png 0690X00000605bLQAQ.png
thibaut by Associate
  • 1095 Views
  • 2 replies
  • 0 kudos

STM32 Nucleo F411RE UART

Posted on July 11, 2016 at 15:50Hello, I am trying to modify the given code for STM32F411RE nucleo board. I want to modify the UARt code by including an interruop section.I have the following code:&sharpinclude ''mbed.h''//--------------------------...

ADC and DAC via DMA

Posted on July 12, 2016 at 14:33Hi,I need to know the exact sequence to be adopted (if any) in order to use the STM32F3xx HAL drivers to implement the ADC multimode conversion with transfer by DMA, using two separate DMA channels for master and slav...

flavio23 by Associate III
  • 856 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.