2016-07-13 8:02 AM
Hi
I set timer 1 for output pwm on a pin.i need when timer is disable, pwm output will have ground level.when output pin is pull up and timer disable,output pin have VDD LEVELwhen output pin is pull down and timer disable,output pin have GND LEVELI SEE ST EXAMPLES PROGRAMS SET PWM OUTPUT PULL UP.NOW IF I SET PULL DOWN , MY DEVICE CORRUPT?? #stm32f4-pwm-output-pin-pull-dow2016-07-13 8:49 AM
Hi jadidi.reza,
You can activate either pull up or pull-down, and this will be fine . Just make the test. -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.