STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

trace in debug

Posted on July 17, 2016 at 21:44Hii want trace my programs(for stm32f429 discovery board) with keil.in my program i used timer1 capture- compar  interrupt. when run program in debug mode  and press F11 my program run to  ISR CONDITION but not go  in...

Code for USART1 on STM32F3-Discovery

Posted on July 16, 2016 at 17:58Clive1 gave a simple code for sending data from the board to the PC via the USB-connection here:/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lis...

johann by Associate
  • 1559 Views
  • 2 replies
  • 0 kudos

Using PB7/6 port of STMF051

Posted on July 15, 2016 at 02:51Hi,I configured USART1 to PA9/10. And I want to use PB6/7 to GPIO.First I initial the USART1 function(using PA9/10), and works well(putchar works well). But when I initial PB6/7 to GPIO by GPIO_Init() function, USART1...

paul0208 by Associate III
  • 1288 Views
  • 3 replies
  • 0 kudos

Stm32F4 Discivery issue to play on boards DAC

Posted on July 12, 2016 at 15:17Hello, I'm new to Stm32 programming, but I try hard. I'm at the bottom of the earning curve and I block since 2 days on the an issue issue. Help would be very much welcomed. I attach my project:https://dl.dropboxuserc...

jmf1 by Senior
  • 1029 Views
  • 1 replies
  • 0 kudos

STM32F767 SPI not sending same data twice.

Posted on July 12, 2016 at 05:18 Hello, Here is my code static void SPI_EnableMaster(SPI_TypeDef *SPIx, uint16_t SPI_CLOCKDIV, uint16_t SPI_MODE, uint16_t SPI_DATA_SIZE, uint16_t SPI_LSBFIRST) { SPI_DATA_SIZE--; SPIx->CR2 = (...

STM32F7: irq flood when using USB HS core in FS mode

Posted on July 15, 2016 at 15:26I just used the USBD_MSC sample from the cube with the F7 Discovery board and configured the HS core to run FS speed only (our own hardware will have no ULPI), therefore changed usbd.conf.c, line 382:   hpcd.Init.spee...

js23 by Associate III
  • 895 Views
  • 0 replies
  • 0 kudos

Flashing Difficulties, Worn Out Flash?

Posted on July 13, 2016 at 20:16I am using Atollic True Studio lite to develop firmware for an STM32F373VCT while using an ST-Link V2 emulator probe. I have noticed that the time it takes to flash the firmware has steadily increased and now I have r...

spflanze by Associate II
  • 2054 Views
  • 4 replies
  • 0 kudos

Mems sensors_datalog is not working

Posted on August 20, 2015 at 14:40I am using NucleoL152RE with X-NUCLEO-IKS01A1 .I loaded x-cube-mems1 Datalog sample code.but that pc suite is not working. #x-nucleo-iks01a1

0690X00000605IYQAY.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.