STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151 stop mode with RTC, 4uA current draw?

Posted on July 21, 2016 at 08:46We use stm32l151ccu6 with RTC clocked by LSI. The device is set to wake up, every 20 seconds,  from stop mode using the RTC auto wakeup feature. At present, the device just goes back to stop mode after clearing the RT...

faizal by Associate
  • 1128 Views
  • 1 replies
  • 0 kudos

STM32Cube Bug - FMC write recovery time

Posted on July 04, 2016 at 12:50STM32CubeMX: 4.15.1 STM32CubeF7: 1.4.0 MCU: STM32F746NGHx In the setting: ''Configuration | FMC | SDRAM1 | SDRAM timing in memory clock cycles | Write recovery time'' the value is constrained in [3,16] (and the help a...

STM32L0 SPI Clock Issue

Posted on July 21, 2016 at 09:55I am using a STM32L053 Discovery board and I am having an issue with the SMI clock line. I am trying to set the device up such that PB13 is the clock lick line (as SPI 2). The problem is that the clock only appears to...

F072 Nucleo TIM2/DMA/Input capture issues

Posted on July 17, 2016 at 08:43 I am trying to work with STM32F072 input capture using TIM2 and DMA transfers. There is an issue in CubeMX which make it always change the alignment to BYTE, I always have to change it back to WORD, really anno...

o2 by Associate II
  • 2487 Views
  • 5 replies
  • 0 kudos

Basic help on ISR's and the HAL

Posted on July 15, 2016 at 22:13 I'm trying to kick off the ADC via Timer1 at 9600 sps for 4 channels. I have it all working -- once, but I think I'm (ab)using the HAL wrong; I tried to put the kick off code in a function in main called ...

stthormj9 by Associate II
  • 3105 Views
  • 6 replies
  • 0 kudos

Help to find Datasheet STM32F301VCT6

Posted on July 19, 2016 at 21:51Hi, firends!!! help me to find Datasheet on such STM32F301VCT6--QFP 100  microcontroller, I not where can't find him, I will be very grateful to you, thanks.

kamal1953 by Associate II
  • 3539 Views
  • 6 replies
  • 0 kudos

STM32F7 TypeDef Error

Posted on July 19, 2016 at 21:53I want to use STM32F767ZI on Nucleo board. I used the ARM GCC in Eclise (Microsoft Windows 10). I wrote following code to test the compiler&sharpinclude <stm32f7xx.h> &sharpinclude ''stm32f7xx_hal.h'' // Sample pragm...

mohsen by Associate II
  • 1283 Views
  • 2 replies
  • 0 kudos

STM32f1xx family MPU table?

Posted on July 20, 2016 at 00:51The Memory Protection Unit (MPU) is a feature that is only implemented in some members of the STM32F1xx family. Is there a simple table which I can peruse to determine which members have the MPU, and which don't have ...

Mikexx by Associate II
  • 1520 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.