2016-07-19 12:06 AM
I am using SPI to communicate with an external NVM memory and hope to have some data validate at the end by using CRC. But I do not understand how does the SPI CRC calculation contribute to verify the data that I transmit and received, can anyone explain?
/*##-1- Configure the SPI peripheral #######################################*/
/* Set the SPI parameters */
SpiHandle.Instance = SPIx;
SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;
SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;
SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW;
SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;
SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;
SpiHandle.Init.TIMode = SPI_TIMODE_DISABLE;
SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE; <-----
SpiHandle.Init.CRCPolynomial = 7;
SpiHandle.Init.NSS = SPI_NSS_SOFT;
2016-07-19 8:25 AM
Hi wy,
As mentioneed in reference manual :''
Hardware CRC feature for reliable communication:–CRC value can be transmitted as last byte in Tx mode
–Automatic CRC error checking for last received byte
'' 32.3.7 SPI onfiguration part describes how to configure the CRC feature. And this part describes how to check the CRC error: ''CRC error (CRCERR)
This flag is used to verify the validity of the value received when the CRCEN bit in the
SPIx_CR1 register is set. The CRCERR flag in the SPIx_SR register is set if the value
received in the shift register does not match the receiver SPIx_RXCRC value. The flag is
cleared by the software.
'' I recommend to have a look to the example in about CRC feature at this path: STM32Cube_FW_L0_V1.7.0\Projects\STM32L073Z_EVAL\Examples\CRC\CRC_Example\Projects\STM32L073Z_EVAL\Examples\CRC\CRC_Example -Hannibal-2016-07-19 9:43 AM
This is for peripherals that support CRC in their SPI protocol.
The SPI could be used to perform a CRC calculation of your data as written if after initializing and sending your whole data stream you would then switch modes and have the SPI peripheral shift out the computed CRC. In the read back case you'd read all your data and the CRC, and then the CRC would be zero (ie division with no remainder). For data integrity in your own memory structures you'd probably want to use a CRC or checksum of your own.2016-07-19 7:41 PM
then probably I would need to change my code, because right now I am sending byte by byte and this caused the CRC generated every byte and the receive data CRC check back incorrect.
This is my code:uint8_t sFLASH_SendByte(uint8_t byte)
{
uint8_t TxBuf[1]; // Buffer used for transmission
memset(TxBuf, 0, 1);
uint8_t RxBuf[1]; // Buffer used for reception
memset(RxBuf, 0, 1);
TxBuf[0] = byte;
HAL_SPI_TransmitReceive_IT(&SpiHandle, (uint8_t*)TxBuf, (uint8_t*)RxBuf, 1);
while (wTransferState == TRANSFER_WAIT)
{
}
wTransferState = TRANSFER_WAIT;
return RxBuf[0];
}
uint8_t sFLASH_ReadByte(void)
{
return (sFLASH_SendByte(DUMMY_BYTE));
}
Currently , I am think using XOR method to XOR all the data that transmitted out and saved the XOR result after the data. Is this method acceptable?
Data the be saved: [byte1][byte2][byte3][XOR byte]
XOR byte = byte1 ^ byte 2 ^ byte 3
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.