STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connect SN65DSI83 LCD to STM32F469

Hi, i'm developing a board with 7" lcd (LVDS) so i'm really hesitating about if is right to use a SN65DSI83 for this, my STM32F469IIT6 only have 2 DSI Lanes. I'm connecting the i2c lane from SN65DSI83 to i2c of STM, i just copied the circuit of cm4-b...

Dallton96 by Associate II
  • 8839 Views
  • 5 replies
  • 2 kudos

Resolved! AN2867 compatible crystal tables

I am currently choosing an LSE and HSE crystal for an STM32H743 project. AN2867 includes tables of compatible STM32 crystals. There is also a crystal selection tool from ECS which i've used. My question is, after selecting a crystal from the tables, ...

BobaJFET by Associate III
  • 1596 Views
  • 1 replies
  • 1 kudos

H7 USB doesn't work with Core WFI

The USB Host seems to not work if WFI is executed in the FreeRTOS Idle task.  Is it not possible to use USB with a WFI Core sleep?Thanks for any insight.  A forum search yielded mention of similar problems on other devices (over years!) but no defini...

Resolved! Reinitialize RTC upon watchdog reset

In my application, I have a watchdog timer that resets every 45 seconds if not fed. I also have an RTC. The application records sensor samples, along with timestamps from the RTC.Problem is, when there is a watchdog reset, the RTC is re-initialized t...

STM32F410RBTX_RAM.ld File Missing

I am using STM32F410RB Nucleo Board for my developement. When I am creating new project chossing the same board STM32F410RBTX_RAM.ld Files is Missing. Due to which I am not able to flash my board and getting error.On the other hand I tried selecting ...

Screenshot 2025-01-23 155801.png

STM32F417 SPI interrupt timing issue

Hello,We have run into some issues regarding SPI in interrupt mode, especially when building with optimizations turned on. We are running SPI at 21MHz.The situation:We transmit one byte using HAL_SPI_Transmit_IT. This immediately triggers a TXE inter...

Untitled Diagram.drawio.png
Marijn25 by Associate II
  • 2286 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H747IGT6 stuck

Hello.I have designed my own STM32H747IGT6 board.And I created a simple project with STM32CubeIDE to confirm its operation.In this project, CM7 is a program that simply blinks the LED in a while loop. (CM4 is just code generation)  while (1) { ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.