2016-11-10 2:59 AM
Hi all,
I'm trying to write a code of a data logger with the following characteristics:I'm employing HAL libs and CubeMx initialization for processor, peripherals, etc. My SDK is Eclipse Kepler with AC6.
The system collapses sometimes and sometimes not, and I don't know why. I've been reading at this forum, and I've found some similar cases, where the system collapses due to interrupts. Other ones (Clive) says that more than 4GB SD cards may causes problems. I don't know why it collapses, and another code without the Queue works properly (but it cannot storage information at the rates I will need). I'm desperate, and the solution is not clear. If someome can help me I will be grateful.Feel free to request code extracts and everyting you want. Thanks and best regards. #problem #stm32 #interrupt #sd2016-11-10 4:34 AM
My issue with >4GB is that you can't use a 32-bit BYTE offset to describe the address. The block device isn't byte addressable, with 512 byte blocks a 32-bit BLOCK address can describe 2TB. ST has an annoying habit of converting back and forth between BYTE and BLOCK values, they fixed the 32-bit limit by using 64-bit offsets, but the conversions are both unnecessary, and if the math is compiled wrong, prone to break.
To get any speed from SD cards you need to write in multiples of 512 bytes, aligned on 512 byte boundaries. Ideally you'd want to write 8KB or 32KB, etc as a single operation, otherwise the command overhead dominates. The erase block size of most current SD cards is the order of 128KB, operations spanning this alignment will be slower. Writing 310 bytes at a time is going to be pretty slow, and compounded if done repetitively.2016-11-10 6:03 AM
Hi clive,
First of all, thanks for your reply.I've been trying to change HAL bsp SD functions (HAL_SD_WriteBlocks and HAL_SD_ReadBlocks), and if I change them, the code stops working. So if the problem were fixed, I will not follow that ''debug'' line anymore.As an actualization, I were using a synchronization after each string, so my process was as follows:Now, synchronization has been removed, and the system works properly. Is it possible that it has been any kind of overflow?. Syncronization is a slow process, so I think that could be a probable issue.
Another test that I will try is to migrate to DMA writing process, so... in your opinion; Could it improve the behavour of the system?.Lots of thanks.2016-11-10 9:49 AM
I'm not a HAL user, I'm using the F4 with SDIO+DMA under the SPL, get multi MBps performance there.
f_sync() will kill performance, shouldn't crash the driver though. Decide a MB or time threshold to do this.Don't use f_printf(). Use sprintf() advancing in a buffer, say 8KB+400 bytes, whenever you hit over 8KB, write the 8KB and then copy any excess to the beginning of the buffer, and start filling again. Remember printf() returns the number of bytes output. So think s += sprintf(s, ''%d\n'', number++);If you have 32KB free, a buffer of that size would be better.2016-11-10 11:17 AM
Thanks again.
I will try to implement a buffer into my code. I hope it gets better performances.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.