2016-12-12 8:03 AM
Hi
You recommand to switch on the board X-NUCLEO-IDB05A1 but i have the X-NUCEO-IDB04A1.
You can see on my previous posts, i'm working for a package for the stm32f746g-disco.
I'll be in holliday at the end of the week Is it possible to provide me a sample as remplacement of the previous board ?
Br,
Christophe
2016-12-13 3:28 AM
Hi,
As a1 is no more in use, May you respond on the point above, please ?
Br,
Christophe
2016-12-13 7:34 AM
Hi Christophe,
the A1 pin on Arduino connector is used for CSN (chip select, active low) both for X-NUCLEO-IDB04A1 and X-NUCLEO-IDB05A1 boards. The software package for both board is the same (X-CUBE-BLE1) and the driver is also the same. The main differences are related to the HCI (Host Control Interface) commands used for BLE communication, where X-NUCLEO-IDB05A1 (based on BlueNRG-MS chip) has more options than the old one.
Kind regards,
Antonio
2016-12-13 10:11 AM
sorry i said a mistake, i was speaking about a4 rev board to a5 .... Not about the a1 pin...
I would ensure to work directly on the latest board.
can you provide a sample of board ?
i ll see about api now.
br Christophe.
2016-12-14 4:11 AM
Hi Christophe,
you can order the board from ST distributors from the bottom of this page ('Sample & Buy' section):
Otherwise you could get in touch with the people that you met at the training in Paris to check if they have any X-NUCLEO-IDB05A1 for you.
In the meantime you can continue using your X-NUCLEO-IDB04A1 board. You will be able to reuse all the code that you are developing as there are no driver differences with the new board.
Hope that helps,
Antonio
2016-12-18 2:25 PM
ok Antonio, I ll check.
Br
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.