STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

An issue about STM32H503 I2C

I'm reading RM0492 Rev 3 about I2C's controller transmitter. The original words on the page of 1185 areWhen RELOAD = 0 and the number of data bytes defined in NBYTES[7:0] is transferred: • In automatic end mode (AUTOEND = 1), a STOP condition is auto...

momo1 by Associate
  • 457 Views
  • 1 replies
  • 1 kudos

Resolved! How to set FDCAN peripheral in STM32H7 NUCLEO Board

Hi, I’m trying to configure the FDCAN peripheral on a NUCLEO-STM32H72ZG board, but even though it works perfectly in loopback mode, it doesn’t work when I switch to normal mode. Even in external loopback, when I check with the oscilloscope I don’t se...

Resolved! H723..H735: functions in ITCM, strange behaviour

Heyho,I recently found that I'm not using ITCM RAM at all, then started to put heap and stack there.No problems so far.Then I copied some functions there, and all went well - until I found some strange behaviour:1..4 SAI RX DMA transfers running, cir...

LCE by Principal II
  • 431 Views
  • 5 replies
  • 2 kudos

STM Virtual Com port win11 driver needed

hello, where can i download win11 STM virtual com port?  i install both VCP_V1.5.0_Setup_w7_x64_64bits and W8_x86_32bit all not working ! i din seeSTM Virtual Com port at device manager! only STM STLink visual com port appear ... 

StanJerm by Associate III
  • 54249 Views
  • 12 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.