2017-01-23 9:27 AM
Hello,
e.g. RM0377 lists the PWR_CR_LPDS bit unconditional for all L0X1 devices. * @version V1.7.1 headers define PWR_CR_LPDS only for L011 and L021. Is this right?
#stm32l02017-01-25 4:14 AM
Hi
Bonnes.Uwe
,In LPDS bit description in
, there is the following note: ' The LPDS bit is available on category 1 devices only'.Category 1 devices are STM32L011xx & STM32L021xx (see table 1 in the reference manual).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.