STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SNMP V3 on STM32f429

Posted on February 01, 2017 at 19:18Hey guysI used this topic:https://community.st.com/0D50X00009XkhwuSAB  and related folders in github and now uclinux is running on my DISCO board.I need to install SNMP-V3 on uc linux. what is the next step and ho...

mehdi2399 by Associate II
  • 1341 Views
  • 1 replies
  • 0 kudos

STEVAL-ISV003V1

Posted on December 30, 2016 at 21:50hey all, i'm currently working on the design of a micro inverter 'STEVAL-ISV003V1' i would like to know more about types of products used in this micro inverter especially the description of capacitors and resisto...

Resolved! How to change VOS bits in 32L0xx

Posted on January 25, 2017 at 08:19Hi,According to reference manual RM0377 (page 138 6.1.5 Dynamic voltage scaling configuration)  programming voltage regulator is very easy. Unfortunately I'm not able to do this on two Nucleo demo boards with STM32...

stm32f2xx DMA re-enabling issue

Posted on February 01, 2017 at 12:25Hi,I'm struggling with the DMA stream reenabling. I'm using 6 DMA streams to transfer known amount of data from memory to periph. Streams are triggerd with two PWM timers in the master-slave mode (update and CC tr...

0690X00000606CCQAY.png
ace0 by Associate II
  • 2433 Views
  • 4 replies
  • 0 kudos

Using TIM3_CH1 to generate a delayed one-shot pulse

Posted on July 30, 2013 at 07:48Hi guys, it's been a few years since I've worked with the timers on these micro's and I've been rediscovering how much of a pain they can be.Please refresh my memory so I at least know whether i'm wasting my time or n...

darcy23 by Associate II
  • 2604 Views
  • 4 replies
  • 0 kudos

Resolved! CubeMX 4.19.0 Problem report.

Posted on January 29, 2017 at 17:22The attached project is made up of CubeMX 4.18.0.If you open the project after opening the project at CubeMX 4.19.0 and then creating source again, an error occurs.

stm32f103 IAP App via gprs

Posted on July 10, 2015 at 11:34I am planning to program stm32f103 micro controller over the air. I have a sim808 module connected for network connections. Any new firmware changes needs to be pushed to the microcontroller via sim808. Can this be ac...

gopalan by Associate
  • 3157 Views
  • 6 replies
  • 0 kudos

nucleo F746zg and ILI9488 TFT

Posted on January 23, 2017 at 07:43Hi,I am trying to use a TFT with ILI9488 via SPI. The Display works but it is incredibly slow. What am I doing wrong ?I am using FreeRTOS and LWip in my project, too.It would be great to get a hint or two.ThanksMar...

Synchronize Micros with independent clocks

Posted on January 31, 2017 at 23:25I want to synchronize micros that each have their own clock. Is that possible? I was thinking of having a Master control the synchronization with GPIO. Essentially, when the pin is high (or low), you start whatever...

Andrew C by Associate III
  • 1254 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.