2017-01-30 11:37 AM
I have a problem with the simultaneous handling of interrupts EXTIx ORAX converter ADC1. I must probe the A / C with a maximum frequency. Therefore, I need to set the maximum possible frequency of the bus APB2. As we increase the frequency of bus APB2 above 4.5 MHz to stop working interrupt eXTix, A/C works. What's wrong? I generate code from STM32CubeMX.
2017-02-01 5:14 AM
It turned out that after changing the frequency APB2, I stopped working properly PWM that controls the system, which generates input signals exti. Enough improvement in the configuration of PWM, the frequency change APB2. Subject shut.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.