STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Creating flow control in VCP-derived code

Posted on March 28, 2014 at 13:41 Dear list, I use the USB-VCP example, from STM32_USB-Host-Device_Lib_V2.1.0, for my application, but am running into some trouble when trying to get the proper flowcontrol for my application. ...

Sietse by Associate III
  • 3930 Views
  • 8 replies
  • 0 kudos

Resolved! Understanding about internal flash

Posted on February 16, 2017 at 10:57Hi ! I want to use STM32L071C8T with 64kbyte flash. But when I see the datasheet, there is 2 bank (32kb each) in the flash and if I am not using dualboot, program is read in bank1. But I am wondering that, if my p...

Use 256KB flash MCU for 210KB code

Posted on February 15, 2017 at 13:29Shall I use STM32L476RCT6 (256KB Flash) MCU for the project which was when compiled on keil shows the total memory equivalent to 210KB.Please Help!!#stm #memory-space #stm32 #stm32l4 #memory

Problems when modifying interrupt vector table in RAM

Posted on February 16, 2017 at 11:06I am working with the STM32F045-microcontroller and I write my source code in Eclipse and I build with GNU ARM C/C++ Cross Compiler and I debug using GDB OpenOCD Debugging with ST-LINK/V2. I have placed the interr...

arnold_w by Senior II
  • 904 Views
  • 1 replies
  • 0 kudos

STM32f429 receiving buffer issue USART DMA

Posted on January 20, 2017 at 12:39Hi,We are using STM32f429 microcontroller for our project.I'm having problem receiving buffer in  USART DMA data between two stm32f429 controllers with the Baud rate of 9600.We are able to receive all the  data eve...

Reading RFID card with STM32f0 series using HAL SPI lib

Posted on February 16, 2017 at 07:23Hello, I am trying to communicate with rfid rc522 using stm32f0 series processor. Spi driver libary is created using cubemx. I am not able to read card id. I tried arduino to receive data from rfid rc522 it is suc...

STM ST-LINK drivers for custom automation tool

Posted on February 15, 2017 at 22:10Hi,We are looking to automate the programming of the .hex file.  Currently we are using the ST-Link tool to manual load then programming the .hex file to the uC.  But we will automate the process using our own sof...

Vu.Andy by Associate III
  • 1009 Views
  • 1 replies
  • 0 kudos

Flashing BlueNRG with my version of Hello World

Posted on February 05, 2017 at 13:11Hello I am new with using the BlueNRG1, so I am having trouble flashing the STEVAL-IDB007V1.  I'm trying to get the binary image to upload it to the BlueNRG and I'm using ATOLLIC TrueSTUDIO to compile my version o...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.