2017-02-15 10:23 PM
Hello, I am trying to communicate with rfid rc522 using stm32f0 series processor. Spi driver libary is created using cubemx. I am not able to read card id. I tried arduino to receive data from rfid rc522 it is succesful. But I could not get any data when ı used stm32f0 series kit. There is something wrong with hal spi libray but ı could not get it.
Here is my main.c
/**
****************************************************************************** * File Name : main.c * Description : Main program body ****************************************************************************** * * COPYRIGHT(c) 2017 STMicroelectronics * * Redistribution and use in source and binary forms, with or without modification, * are permitted provided that the following conditions are met: * 1. Redistributions of source code must retain the above copyright notice, * this list of conditions and the following disclaimer. * 2. Redistributions in binary form must reproduce the above copyright notice, * this list of conditions and the following disclaimer in the documentation * and/or other materials provided with the distribution. * 3. Neither the name of STMicroelectronics nor the names of its contributors * may be used to endorse or promote products derived from this software * without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 'AS IS' * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE * FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL * DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER * CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ****************************************************************************** *//* Includes ------------------------------------------------------------------*/#include 'stm32f0xx_hal.h'#include 'spi.h'#include 'gpio.h'#include 'rc522.h'#include 'stm32f0xx.h'/* USER CODE BEGIN Includes *//* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*//* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);void Error_Handler(void);/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*//* USER CODE END PFP */
/* USER CODE BEGIN 0 */
uint8_t data_get[10];uint8_t data_received[10];uint8_t data_send= 55;uint8_t recdata;/* USER CODE END 0 */int data_receive_flag=0;uint8_t CardID[5];int counter =0;uint8_t send[3];uint8_t dum=0xFF;;//My cards id
int main(void){/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* Configure the system clock */
SystemClock_Config();/* Initialize all configured peripherals */
MX_GPIO_Init(); MX_SPI1_Init(); /* USER CODE BEGIN 2 */ init(); /* USER CODE END 2 *//* Infinite loop */
/* USER CODE BEGIN WHILE */while (1)
{ if(isCard()) { data_receive_flag = readCardSerial(); if(readCardSerial()) { data_receive_flag = 1; } } } /* USER CODE END 3 */}/** System Clock Configuration
*/void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 16; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); }RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); }HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
}/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence. * @param None * @retval None */void Error_Handler(void){ /* USER CODE BEGIN Error_Handler */ /* User can add his own implementation to report the HAL error return state */ while(1) { } /* USER CODE END Error_Handler */ }#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */ /* USER CODE END 6 */}
#endif/**
* @} *//**
* @}*//************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
Here are my spi rc522 libraries added
Is anyone help me?.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.