STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MatTarget 4.4.1 DEMO Model error

Posted on February 15, 2017 at 14:40   Hello:I am trying the demo model STM32F407_DAC.slx in folder STM32-MAT\STM32\STM32demos\Test\DAC\, when I compile this model, there are pop up two windows as follow: but I check the .ioc file no problem.My soft...

0690X00000606H8QAI.png

STM32L4 FreeRTOS MPU Support Question

Posted on February 14, 2017 at 18:28I read that full FreeRTOS MPU support is available on the Cortex M3, and the M4F.  The STM32L4 is advertised as being a Cortex M4 (without the 'F'), so my question is, does FreeRTOS provide full MPU support for th...

Accuracy of on board A/D STM32L0

Posted on February 15, 2017 at 14:21Hi,   I am just coming from anothr controller and learning the different parts of the STM32L0 for low power applications.  I am about to start on the 12bit A/D, which hopefully will save me having to add an extern...

NMI Handler on STM32F091 on debug

Posted on February 15, 2017 at 12:56Hi all,I'm trying to set-up the USART interface.. Very complicated.. but on the debug if I insert a breakpoint on the USART1_IRQHandler the program goes to NMI_Handler.. Why? Thanks a lot.

PWM glitch

Posted on February 14, 2017 at 13:28 Hi, I'm using the PWM to create a sinusoid at a desired frequency and amplitude. I have a table with the values, and I am updating it during the execution of the program. But I have an unexpected glitch th...

0690X00000602QyQAI.bmp 0690X00000602R3QAI.bmp

STM32F407 AND FREEZ IWDG

Posted on February 06, 2017 at 14:01Hello could you show me example how to stop or freez IWDG in STM32F407 ?Thank you in advanced

STM32F427 CAN Data Check

Posted on February 13, 2017 at 16:30I am currently running CAN1 and CAN2 on the F427 and need to check/validate the Transmitted Data.Both CAN1 and CAN2 function correctly.I wish to Transmit Data on CAN1 and, if possible, Receive the sent Data in the...

High Quality Audio I/O

Posted on February 15, 2017 at 01:52I can use one SAI  RxTx channel  or Two separate SAI ports,  providing independent Rx and Tx channels.Which solution supplies the best HD stereo audio quality ?My processor board is based on the STM32F7The design ...

T J by Lead
  • 763 Views
  • 0 replies
  • 0 kudos

No variables showing on STM-studio (IAR)

Posted on October 09, 2014 at 09:22Hi all,I'm having troubles connecting the STM-studio with the STM32F4 - Discovery.I am using STM-studio 3.3 with IAR Embedded Workbench for ARM (7.3) and after debugging and importing the c.out file, It only shows ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.